Results 1 to 6 of 6

Thread: the right controller

  1. #1
    Join Date
    Sep 2008
    Location
    Edmonds, WA
    Posts
    148
    Rep Power
    38

    the right controller

    Hello,
    I'm thinking about making a biped robot but don't know what microcontroller to use.
    I have no programming experience(even struggling with roboBASIC) but I'm planning on learning BASIC by myself.
    I was thinking BotBoard II or Axon but any suggestions?

    Thanks

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    125

    Re: the right controller

    What type of servos? Standard hobby servos, or something serial based like Bioloid Ax-12s?

    Also, what do you intend to have the robot do? Do you want to make it autonomous, or are you just going to control it wirelessly (and by PC or via a PS2 controller or the like....)?

    -Fergs

  3. #3
    Join Date
    Sep 2008
    Location
    Edmonds, WA
    Posts
    148
    Rep Power
    38

    Re: the right controller

    Thanks for the reply
    It's going to be autonomous and will have about 6~8 analog servos

  4. #4
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    125

    Re: the right controller

    Quote Originally Posted by xx2747 View Post
    Thanks for the reply
    It's going to be autonomous and will have about 6~8 analog servos
    So pretty much an autonomous BRAT (http://www.lynxmotion.com/Product.as...&CategoryID=97), in which case, the BotBoard II will probably be sufficient as that is what ships with it....

    While I would normally be a huge advocate of the AVR architecture, the Axon would almost certainly require you to use C, rather than BASIC (any particular reason you want to do BASIC?). It's also probably overkill for such a project, something along the lines of an Arduino could suffice for 6 servos (hmm.. maybe a Roboduino http://www.trossenrobotics.com/roboduino.aspx). But again, you'd be using C.

    -Fergs

  5. #5
    Join Date
    Sep 2008
    Location
    Edmonds, WA
    Posts
    148
    Rep Power
    38

    Re: the right controller

    Thanks,
    But what's the difference between C and BASIC?
    Is there a particular reason I should start out with BASIC if I don't know anything about programming?
    I don't know if BBII will support HS-81s though.

  6. #6
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    174

    Re: the right controller

    It'll support any PWM driven servo.

    As far as C vs BASIC, that's years worth of posting. I'd suggest Google.
    I Void Warranties´┐Ż

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. RC & Serial Servo Controller Kit
    By Al1970 in forum Garage Sale
    Replies: 0
    Last Post: 01-10-2009, 12:39 AM
  2. Question(s) Motor Controller. Do I need a servo controller too?
    By kankatee in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 11-14-2008, 10:03 AM
  3. Question(s) Motor controller ?'s
    By sthmck in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 11-06-2008, 03:29 PM
  4. Controlling Servos with a servo controller
    By bodhibuilder in forum Arbotix, Microcontrollers, Arduino
    Replies: 25
    Last Post: 09-29-2008, 11:07 AM
  5. Contest Entry Digital Slot Car Controller
    By wrighthobbies in forum Project Showcase
    Replies: 1
    Last Post: 09-21-2007, 01:05 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •