Results 1 to 5 of 5

Thread: Solar NiCad charging

  1. Solar NiCad charging

    I am wanting to set up a circuit to charge two batteries via a solar cell and I can't find a whole lot of good information on it.

    I found this:

    http://www.solorb.com/elect/solarcir...rge/index.html

    but I don't quite understand how that doesn't overcharge the batteries. A fully charged NiCad is around 1.5 volts (so two would be 3v), but 7-solar cells will give 3.5 volts. So left alone wouldent that over charge it?

    I also assume the resistance of the battery while charging increases, but I cant find anything that talks about the charging characteristics, only discharging.

    I have done some poking around but all I can find is information on how to charge the batteries assuming you have a charger. I want to know the theory behind the charging/charger to make my own solar charger.

    Thanks!

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: Solar NiCad charging

    The current is so low, its effectively a trickle-charger. I think that most NiCD/NiMH cells can pretty much trickle-charge for a long time without adverse effects.

    -Fergs

  3. #3

    Re: Solar NiCad charging

    I read so too; when you trickle charge a NiCd battery, you could keep it plugged/charging for a long time without harming the cell.
    The trickle charge delivery recommended is at the highest a 10th ampere an hour of the battery's ampere.

    P.S - I think a NiCd cell's voltage is 1.2 V.

  4. Re: Solar NiCad charging

    I guess the current is what I am a little confused about.

    I assume the battery acts as a resistor as it is being charged (?) but I cant find anything that talks about the behavior of a battery as it is being charged.

    So I know to trickle charge, the current should be less than C/10. What I would like is some way to actually estimate what the current is, short of hooking up a amp meter after the circuit is built.

    I also don't see anything that says what voltage my source should be to charge a nicad cell. I know it has got to be more than 1.2v, but how much more?

  5. #5
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: Solar NiCad charging

    With a solar charger, the current is a function of the panels themselves -- and furthermore, a function of the amount of sunlight falling on them.

    -Fergs

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. A really clever charging solution
    By archcvd in forum Power
    Replies: 9
    Last Post: 09-22-2008, 03:31 AM
  2. solar powered robots
    By openmindedjjj in forum Robotics General Discussion
    Replies: 10
    Last Post: 07-24-2008, 11:36 AM
  3. charging and battery system
    By asbrandsson in forum Robot Computers
    Replies: 1
    Last Post: 01-29-2008, 04:54 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •