Page 1 of 29 123451126 ... LastLast
Results 1 to 10 of 290

Thread: EX-106+/RX-64 Humanoid Robot: Giger

  1. #1
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    EX-106+/RX-64 Humanoid Robot: Giger

    As some of you may already know, I ran into some pretty major issues with Hagetaka walking correctly. Mostly it boils down to too much payload, and the hip-roll servos needing to be upgraded to EX-106s to compensate. I had Hage walking, but the feet were dragging and causing it to veer off course, which I was not happy with. Not wanting to be without a bot for Year 1 Mech Warfare, I decided to go with a backup plan I had cooking. Browse: Supercheap Catalogue and Aldi Catalogue on Catalogue AU.

    3 days of insane amounts of CNC work later... I have Giger:

    Giger Beta v0.1:


    Giger Beta v0.5:


    Giger v1.0 (RX-64/RX-28 version):


    Giger v2.0 (EX-106/RX-64/RX-28 version):


    Giger v2.5 (EX-106/RX-64/RX-28 Mech Warfare variant):


    Giger v3.0 ('Giger Fu' EX-106/RX-64/RX-28 version):


    Giger v3.5 ('Giger Fu' EX-106/RX-64 version):
    Last edited by DresnerRobotics; 01-31-2011 at 03:21 PM.

  2. #2
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    84

    Re: RX-64 Humanoid: Giger

    WoW! Thats awesome!

    Really massive humanoid. I'm guessing that its not only I that envy you all those 64's...
    Excellent built again!

    Looking forward to see him walking.

    -Zenta
    Last edited by Zenta; 05-31-2009 at 03:57 PM.

  3. #3
    Join Date
    Mar 2008
    Posts
    310
    Images
    49
    Rep Power
    56

    Re: RX-64 Humanoid: Giger

    Just wow! For some reason, I especially like the head, I have no idea why. (but it needs menacing led eyes :P)

    And I am shocked that the RX 64's had such a thing as too much payload!

  4. #4

    Re: RX-64 Humanoid: Giger

    Wow ! It's amazing to me you can crank out such a great looking mech in such short order.

    It's a shame that Hagetaka didn't work like you'd hoped. I loved the whole MechWarrior look. Can you describe in more detail the issues you ran into ? What motion does the 'hip roll' servo provide ? Hip roll, I guess, but I don't which hip motion that corresponds to.

    Thanks,
    CogswellCogs
    Last edited by CogswellCogs; 06-01-2009 at 01:20 AM. Reason: mispelling

  5. #5
    Join Date
    Feb 2009
    Location
    Mesa, AZ
    Posts
    351
    Images
    84
    Rep Power
    53

    Re: RX-64 Humanoid: Giger

    HATCHETMAN!!!


  6. #6
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Re: RX-64 Humanoid: Giger

    Quote Originally Posted by CogswellCogs View Post
    Wow ! It's amazing to me you can crank out such a great looking mech in such short order.

    It's a shame that Hagetaka didn't work like you'd hoped. I loved the whole MechWarrior look. Can you describe in more detail the issues you ran into ? What motion does the 'hip roll' servo provide ? Hip roll, I guess, but I don't which hip motion that corresponds to.

    Thanks,
    CogswellCogs
    Thanks guys (and gals)!

    In most humanoids all the servos are named depending on which axis they are on. Ankle-Roll, Ankle-Pitch, Knee-Pitch, Hip-Pitch, Hip-Roll, Hip-Yaw. Think aerodynamics terminology. The Hip-Roll & Ankle-Roll are the servos that shift the weight from side to side. Hagetaka could shift the weight no problem, but when the lifting foot would raise up, the opposite Hip-Roll servo wasn't strong enough to keep the hips parallel to the ground, and they would sag. If I tried to overcompensate for this, the servos would stall completely. This resulted in the robot dragging its lifting foot across the ground with each step it took, which in turn caused it to veer off course and walk in a very crippled fashion. I was not happy with it at all, thus the rather drastic last minute reconfiguration: I'll very likely revisit Hagetaka when I don't have a competition in less than 2 weeks.

    So far Giger is about 1kg lighter than Hagetaka. It's a 22DOF humanoid, 16 RX-64s and 6 RX-28s. Airsoft guns are going to be mounted on the side of the forearms. I'll have full pan/tilt for aiming, as well as being able to toggle finer arm aiming.

    Sienna- I'm actually going with a red Cylon type eye

    Manny- I actually thought the same exact thing, though it wasn't intentional

  7. Re: RX-64 Humanoid: Giger

    I just have to say...SWEET!

  8. #8
    Join Date
    Feb 2008
    Location
    California
    Posts
    421
    Images
    33
    Rep Power
    54

    Re: RX-64 Humanoid: Giger

    Just curious, what were you using to power up your RX-64s? I'm wondering if it's a power issue since the spec on the 64 is a beastly 888 oz/in at 15V!!!

    Were you using LiPo technology to source the tremendous amount of current that the RX-64s combined will need?
    ---
    Sleep? You don't need sleep...

    ---

  9. #9
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Re: RX-64 Humanoid: Giger

    Quote Originally Posted by tom_chang79 View Post
    Just curious, what were you using to power up your RX-64s? I'm wondering if it's a power issue since the spec on the 64 is a beastly 888 oz/in at 15V!!!

    Were you using LiPo technology to source the tremendous amount of current that the RX-64s combined will need?
    Actually I was using a 5S LiPo, which caps at about 21v (max voltage spec for the RX-64s, puts them over 1000 oz-in of torque).

    Gotta keep in mind though, Hagetaka had 5 lbs of payload on top of those legs and a very wide leg stance, which was ultimately the problem. Upgrading the hip-roll and ankle-roll servos to EX-106s is probably my next step to getting that project back on track, but I can't afford 2 grand worth of servos given the considerable amount I've already put into this.

    New forearms:

    Last edited by DresnerRobotics; 06-05-2009 at 10:09 AM.

  10. #10
    Join Date
    Sep 2008
    Posts
    60
    Images
    2
    Rep Power
    46

    Re: RX-64 Humanoid: Giger

    Nice!
    He'll be like Zyn's little brother!

Thread Information

Users Browsing this Thread

There are currently 12 users browsing this thread. (0 members and 12 guests)

Similar Threads

  1. Contest Entry Hockey Playing Humanoid
    By RobotGrrl in forum Project Showcase
    Replies: 13
    Last Post: 01-14-2009, 05:20 PM
  2. Help for beginner- Humanoid
    By mclayj in forum Robotics General Discussion
    Replies: 7
    Last Post: 09-22-2008, 09:21 AM
  3. humanoid beginner
    By Raul in forum Humanoids, Walkers & Crawlers
    Replies: 15
    Last Post: 06-17-2008, 06:52 PM
  4. Humanoid or Johnny 5 for research
    By musashi in forum Robotics General Discussion
    Replies: 14
    Last Post: 01-12-2008, 08:06 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •