Page 3 of 29 FirstFirst 12345671328 ... LastLast
Results 21 to 30 of 290

Thread: EX-106+/RX-64 Humanoid Robot: Giger

  1. #21
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    102

    Re: RX-64 Humanoid: Giger

    The gripper is pretty sweet. Any plans on releasing an AX-12 version?

    DB

  2. #22
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Re: RX-64 Humanoid: Giger

    Quote Originally Posted by darkback2 View Post
    The gripper is pretty sweet. Any plans on releasing an AX-12 version?

    DB
    I'm not really in the robot parts manufacturing game personally

    I could very easily design an AX-12 version and publish the drawings though.

  3. #23
    Join Date
    Jan 2008
    Location
    Montreal, Canada
    Posts
    477
    Images
    63
    Rep Power
    60

    Re: RX-64 Humanoid: Giger

    Pretty cool Mech you have there!

    Congrats!

    I'd love for my (yet to be built) mech to destroy yours

    Sam

  4. #24

    Re: RX-64 Humanoid: Giger

    I feel split. Part of me wants to see that mech work, and then maybe not.
    'Cuz seeing that mech makes me really scared.

    And then... I remember that I'm in the hex league (phew!)
    Way to go, keep it up!

    @sam
    What type of mech are you planning to build? Biped? Quad? Maybe even Hex?

  5. #25
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Re: RX-64 Humanoid: Giger

    There will be an Open League as well, where everything can battle it out

  6. #26
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Re: RX-64 Humanoid: Giger

    I'll try to get some video up this week, I promise! I've made a lot of progress on this over the weekend.

    Also, figured I would share some prototype hands I'm working on. These should be completely doable on my CNC, but I'm also looking at just using roller chain for the fingers as well. Currently this design needs to be scaled down a bit, but it's a start.







    And a 3 finger version as well:



    They would use zipties running down the inside of each finger, coming through a slot on the back of the hand and attached to the servo hinge bracket, still a work in progress and I'll likely scale them down a bit. Inspiration and design pulled from the "Melissa Hands"
    Last edited by DresnerRobotics; 09-21-2009 at 02:16 PM.

  7. #27
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    181

    Re: RX-64 Humanoid: Giger

    When do we get to see him walk?
    I Void Warranties´┐Ż

  8. #28

    Re: RX-64 Humanoid: Giger

    If the hand becomes too destructive (if at all), will it be declared hardcore? I mean, it IS an RX-64 powered hand. I saw the demonstration/"Public safety warning" video.

  9. #29
    Join Date
    Nov 2007
    Posts
    397
    Images
    71
    Rep Power
    56

    Re: RX-64 Humanoid: Giger

    the zipties would probably snap

  10. #30
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Re: RX-64 Humanoid: Giger

    Quote Originally Posted by MSK Mech Commander View Post
    If the hand becomes too destructive (if at all), will it be declared hardcore? I mean, it IS an RX-64 powered hand. I saw the demonstration/"Public safety warning" video.
    It's just an RX-28 in there actually, and it's not really intended for strength. I have a straight up gripper that is more functional, this is mostly for aesthetics and the challenge of building it.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry Hockey Playing Humanoid
    By RobotGrrl in forum Project Showcase
    Replies: 13
    Last Post: 01-14-2009, 05:20 PM
  2. Help for beginner- Humanoid
    By mclayj in forum Robotics General Discussion
    Replies: 7
    Last Post: 09-22-2008, 09:21 AM
  3. humanoid beginner
    By Raul in forum Humanoids, Walkers & Crawlers
    Replies: 15
    Last Post: 06-17-2008, 06:52 PM
  4. Humanoid or Johnny 5 for research
    By musashi in forum Robotics General Discussion
    Replies: 14
    Last Post: 01-12-2008, 08:06 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •