Results 1 to 4 of 4

Thread: Another person with Roboard questions

  1. #1
    noob Guest

    Another person with Roboard questions

    I've been looking over the Roboard, and I think it may be the product I'm looking for. I want to make an ultramobile UAV, so mostly I'm looking at controlling up to four brushless DC motors, as well as reading in data from an accelerometer.

    I havn't been able to tell from reading the Roboard's documentation; can you connect servos and motors directly to the board and control them, or do you have to also have servo / motor controllers? If you can hook them directly up, do they draw their power from the board, or do you have to wire them to power seperately? And since the board seems to apply the same voltage to everything, would I need to get motors and servos that can operate on the same voltage safely?

    Sorry of the questions are elementary, I just couldn't find the answers anywhere else.

    Thanks!

  2. #2

    Re: Another person with Roboard questions

    While the roboard may very well be the right answer for you (I can't tell you that, as I've never used one, sorry).

    But since you are looking into the UAV scene I thought I'd toss out http://www.diydrones.com

  3. #3
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    126

    Re: Another person with Roboard questions

    Quote Originally Posted by noob View Post
    I've been looking over the Roboard, and I think it may be the product I'm looking for. I want to make an ultramobile UAV, so mostly I'm looking at controlling up to four brushless DC motors, as well as reading in data from an accelerometer.

    I havn't been able to tell from reading the Roboard's documentation; can you connect servos and motors directly to the board and control them, or do you have to also have servo / motor controllers? If you can hook them directly up, do they draw their power from the board, or do you have to wire them to power seperately? And since the board seems to apply the same voltage to everything, would I need to get motors and servos that can operate on the same voltage safely?
    You can control servos directly. To control motors, you'll have to interface an external motor controller (probably one that takes servo pulses? you'll probably have to get an RC motor controller, your choices might be limited based on the need for brushless). The V+ line for each servo does draw power from the board, but will be fed whatever voltage you feed to the roboard.

    One recommendation I would make, is to use digital servos which can hold their position after being given a single pulse (you don't have to update the pulse train continuously, which is a little bit of a pain to do with the Roboard API).

    Edit to add: although really, in a UAV, realtime is fairly important.... I'd think a microcontroller, even a higher end ARM, would be a better solution....

    -fergs

  4. #4
    noob2 Guest

    Re: Another person with Roboard questions

    Hi, I've been wanting to use Roboard as a servo controller too of 3 independent servos. Now that I know I could control servos directly using Roboard, I need to start programming the interface. Can anyone tell me what libraries I should use, and how to compile the codes for Roboard to run? It'll be great if any of you can share some sample codes on servo control with me too. Thanks.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Roboard questions
    By mx270a in forum Robot Computers
    Replies: 13
    Last Post: 07-23-2009, 11:43 AM
  2. Roboard Questions
    By sniperscope in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 05-07-2009, 12:19 PM
  3. Weapon questions
    By Alucard in forum Mech Warfare
    Replies: 35
    Last Post: 02-14-2009, 06:44 PM
  4. Replies: 24
    Last Post: 07-30-2008, 03:31 AM
  5. Scorpion Mini question(s)
    By xyzzy1126 in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 02-21-2007, 04:26 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •