Results 1 to 5 of 5

Thread: Accelerometer

  1. Accelerometer

    I need to measure vibration of a rotating cylinder but I am not sure of the type of accelerometer to use. It may also be used for other measurements so I don't want a vibration sensor. I need some advice on what frequency and g range would work for vibration.

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    174

    Re: Accelerometer

    Welcome to the forum!

    I suspect we'll be needing more information than that. A 20meter, 12 Ton steel cylinder rotating at 1 rotation per month would have a very different signature than would a 2mm, 3g Delron cylinder rotating at 30,000RPM.

    Even with that, we'd be guessing - but at least our guesses will be somewhere in the "educated" realm.
    I Void Warranties´┐Ż

  3. Re: Accelerometer

    Sorry for my vagueness. I am rotating a set of aluminum cylinders with a height of 60 cm. There is an outer cylinder with a radius of 22 cm and an inner cylinder with between 11 and 21 cm depending on the setup. The cylinders are then filled with water and rotated at a max 2000 rpm. The total weight of the rotating part of the instrument is around 450 lbs. I need to measure the vibration for quality purposes but I am not sure of the g forces that would occur during vibration. I would assume that I would need a minimum frequency to cover the rotational speed which would be around 34 Hz. I would guess that 200 Hz would work fine but I am uncertain of the possible vibrational g forces. Maybe 5-10 g.

  4. #4
    Join Date
    Jul 2008
    Location
    Belgium
    Posts
    633
    Images
    2
    Rep Power
    60

    Re: Accelerometer

    Analog devices has an entire range of accellerometers, some of which might meet your needs.
    However, they top off at 2.5kHz bandwidth so I think you'll be pushing them. There might very well be a higher frequency vibration than the 2000rpm rotation.

    Is there a way you can just slap on a simple piezo beeper on there and hook up an oscilloscope to get a rough estimate of the frequency without too much expense? (see the mechwars hit sensor for example)
    Artificial Intelligence is no match for Natural Stupidity

    "For a list of all the ways technology has failed to improve life, press three" - Alice Kahn

    Resistance is futile! (if < 1)

  5. Re: Accelerometer

    What sort of interface are you looking for? A simple analog output that you can feed into something, or something like USB?

    I have a sample program that reads acceleration in from a Phidget 3 axis accelerometer http://www.phidgets.com/products.php?product_id=1059, ran it through a software highpass filter to get rid of anything under 4 hz, does a FFT to it in order to show the frequency components, and then graphs it. It was pretty reliable up to a few hundred hz. The sensor is a little noisy, but there's a new one coming out shortly that's a lot better.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Triangles Rule!
    By Sienna in forum Humanoids, Walkers & Crawlers
    Replies: 54
    Last Post: 05-13-2009, 08:08 PM
  2. Question(s) Pan-tilt + accelerometer(?)
    By javafiend in forum Sensors
    Replies: 2
    Last Post: 04-10-2009, 03:19 PM
  3. weather proof accelerometer
    By Researcher in forum Sensors
    Replies: 0
    Last Post: 01-29-2009, 03:53 PM
  4. RAS-2 Accelerometer English Manual
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 06-06-2008, 11:25 AM
  5. Using accelerometers in VB6
    By Mooncinder in forum Software and Programming
    Replies: 5
    Last Post: 03-07-2007, 08:10 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •