Page 1 of 2 12 LastLast
Results 1 to 10 of 13

Thread: The new Arduino Wheeled Robot kit

  1. The new Arduino Wheeled Robot kit

    Hi all

    We guys on the other side of the ocean got a new Arduino Wheeled Robot kit from Inex.



    It is here http://robosavvy.com/store/product_i...roducts_id/547

    What is your opinion on it? I do find it a nice proposal considering the price.

    Are you guys getting it on trossen as well?

    Also, in my case I was considering using an I2C compass for navigation but someone was saying that these are very prone to errors when we hit bumps...
    Is this a fact? What is your opinion on it?

    Regards
    Pedro

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: The new Arduino Wheeled Robot kit

    Personally, it looks like a not-so-clean, and slightly more expensive version of the 3PI... it appears some of the I/O may be brought out better though (which is my main gripe with the 3PI, you can attach say a GP2D12 to it without soldering)...

    -Fergs

  3. #3
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    173

    Re: The new Arduino Wheeled Robot kit

    Wow. Do you want an honest opinion? This is a shipping commercial product and not something put together by a first-time robot builder?
    I Void Warranties´┐Ż

  4. #4
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: The new Arduino Wheeled Robot kit

    Quote Originally Posted by PedroR View Post
    Also, in my case I was considering using an I2C compass for navigation but someone was saying that these are very prone to errors when we hit bumps...
    Is this a fact? What is your opinion on it?
    Ok, so on the robosaavy site they have this quote: "Add an I2C compass and it will always know where it's headed" I don't even know where to start here. That's so entirely untrue. A digital compass, like any compass, but especially the digital ones, will be thrown off by any magnetic field. A robot, has tons of (time-varying) magnetic fields. Unreliable when "we hit bumps" is probably more of an issue that the robot's motors have to pulse up, causing a magnetic field that throws off the compass. Or, it might be that the compass dips out of the horizontal plane. Either way, a digital compass will not make it so your robot "always knows where it's headed". You'll have to add back end processing to keep track of where the robot has been, what the readings were, and what the motor outputs have been, then you can, with some probabilistic certainty know where you are headed.... Unfortunately, there are no magic sensors out there, they all have issues.

    -Fergs

  5. #5
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    138

    Re: The new Arduino Wheeled Robot kit

    As the 'buyer' for Trossen, I don't see much point in picking it up when we already carry the 3pi. It's more expensive and nowhere near as polished. As Fergs said, the only thing about the 3pi is that the I/O isn't as easily accessible, however a $20 breakout board fixes that, and it would still be less expensive.

    I'm sure some people out there will like it, but it fills the same slot as the 3pi for us, and we try not to overlap products too much.

  6. Lightbulb Re: The new Arduino Wheeled Robot kit

    Hi guys

    Thanks for all your feedback.

    It was very important for me to understand a number of things.
    Let me explain:

    1) The main target of the product is actually the Education Market. The manufacturer (Inex) has a very broad portfolio of robot kits for education. (maybe that's why the kit comes with such bright colours.... LOL): All sensors (the included ones and the optional ones) use JST connectors to avoid the need for soldering; it also comes with activities manuals that help teachers and students learn with the robot, etc.

    We actually have another kit from them (similar but based on ATMEGA8 with less option parts/extras) which is quite popular.



    2) From your comments I now understand this platform isn't very appealing to power users given there is the 3pi.
    Indeed the 3pi is a very nice product - and surelly much better suited for power users given the great quality DC motors it employs - but it is not RoHS complaint and thus it is a serious risk to sell it in Europe (so we can't really do it).



    3) As for the compass and other navigation techniques, this issue has also been brought up in the Robosavvy forum.
    I've learned that a gyro is an important addition to these platforms to account for all the issues of not navigating levelled: the issues with the compass that you mention, the issues when you go over a bump where the actual horizontal distance is less than the one measured by the wheel, etc.
    A wheel encoder is also something that was mentioned but that option exists for these robots.
    This combination was aimed at using "gyrodometry".

    Someone also mentioned the use of Accelerometers although I still don't understand how you sue the information from these. Are they to account for the cases when only one wheel slips and you have centrifugous acceleration?

    A final mention to the Arduino board it includes: the board is a bit expensive when purchased stand alone but it does expose all IO nicelly as Inxsfergy noticed. This one adds for example, support/connectors for 2 PWM servos in addition to the 2 dc motors; not sure about the 3pi though; probably has it was well.

    As a sidenote pricewise you guys in the US usually get better end user prices. In Europe we always end up with higher end user prices mostly due to the heavvy VAT which in our case makes prices 15% more expensive...

    Once again, thank you all for your feedback.

    And Andrew, thank you too. I hope we can keep talking on both forums

    Regards
    Pedro.
    Last edited by PedroR; 07-03-2009 at 11:59 AM.

  7. #7

    Re: The new Arduino Wheeled Robot kit

    I've been researching various controllers, and ran across the RoboDuino as an Arduino clone. I am hoping there will come kits based on the RoboDuino since it is designed for robotics and has all the nice 3 pin headers for sensors and devices. This should solve some of the short comings of using Arduinos for robotic projects. I'll eventually be using one or more RoboDuinos for specific processing tasks on my robot.

    8-Dale
    I can handle complexity. It's the simple things that confound me.
    Do everything in moderation, ESPECIALLY, moderation..
    Sometimes the only way to win, is not to play.. -- Stephen Falken

  8. #8
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    138

    Re: The new Arduino Wheeled Robot kit

    Yup we carry the Roboduino here, I prefer it over the Arduino simply for ease of use. No need to breadboard; sensors and servos can plug right in.

  9. #9

    Arrow Re: The new Arduino Wheeled Robot kit

    Quote Originally Posted by Tyberius View Post
    Yup we carry the Roboduino here, I prefer it over the Arduino simply for ease of use. No need to breadboard; sensors and servos can plug right in.
    Yep! I'll probably get one of them next month. I've been wanting to use an Arduino for robotic projects ever since I got my first one, but the fact of not being able to connect standard servos and sensors to it easily has put me off from doing that.

    I've done some breadboarding with my Arduino and Sanguino, and have had servos connected to them, but I consider it a pain to wire everything up. I've had my Arduino connected to up to 6 servos so far and written what I consider a better software PWM library. The RoboDuino will make this MUCH easier and I'll be using one to handle processing for my 3-axis accelerometer and other things for W.A.L.T.E.R.

    8-Dale
    I can handle complexity. It's the simple things that confound me.
    Do everything in moderation, ESPECIALLY, moderation..
    Sometimes the only way to win, is not to play.. -- Stephen Falken

  10. #10
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: The new Arduino Wheeled Robot kit

    Quote Originally Posted by LinuxGuy View Post
    I've had my Arduino connected to up to 6 servos so far and written what I consider a better software PWM library.
    Take a look, but the new Arduino 0017 release includes a hardware servo library that can control 12 servos.

    -Fergs

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 09:20 AM
  2. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •