Page 2 of 2 FirstFirst 12
Results 11 to 15 of 15

Thread: Motion sensor controlled Tilt and Pan Camera (wireless)

  1. Re: Motion sensor controlled Tilt and Pan Camera (wireless)

    Thanks guys this is all really helpful!!

    I'll Keep you updated with project and might come back if i need more help thanks again really appreciated!!

    I'll also post my results thanks


    ACEX

  2. Re: Motion sensor controlled Tilt and Pan Camera (wireless)

    Wondering about the range to theXbee Starter Kit, it say 100 meters... likelyhood is that my plane is gonna go way beyond that.... anyway I can boost it??

  3. #13

    Re: Motion sensor controlled Tilt and Pan Camera (wireless)

    There are different versions of the xbee modules they range from the short range (included with the kit) to 900mhz versions with lower data rates but distances up to 6 miles check out the 60mW it has an approx 1 mile range. You can piece together the same items as the kit except using the 60mW xbees and get 1 mile range.

    http://www.trossenrobotics.com/store...onnection.aspx

    Also the antenna will affect range
    Last edited by nagmier; 07-03-2009 at 07:07 PM. Reason: Link addition and another comment

  4. #14
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    182

    Re: Motion sensor controlled Tilt and Pan Camera (wireless)

    Yeah, and planes are in a much more best-case scenario. With an antenna on a building, bot on the ground, even the shortest range xbees will reach out 500+ ft. The airplane has a large look/footprint between it and the ground.

    Lowering the datarate also raises the reliability and distance. You surely don't need more than 2400bps for two servos!
    I Void Warranties´┐Ż

  5. Re: Motion sensor controlled Tilt and Pan Camera (wireless)

    Okay, I dont know if this will help or not, BUT (LOL) I have been tossing around building a mech for the Mechwar Games in 2k10. I was considering using such a setup as my pan/tilt on the torso and did some research on hardware. I was able to find these if they help any:

    http://blog.makezine.com/archive/200..._gyroscop.html
    http://hobbywireless.com/cart/index....index&cPath=31


    If you wish to slap me now I wont run much LOL. I am at work and way to tired.

    They plug into the RC Transmitter as another channel on the trainer link or something like that.
    Last edited by WarriorofHonour; 07-08-2009 at 04:30 AM. Reason: Added info

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Pan, Tilt, Roll, Zoom, Shutter
    By Envision in forum Projects For Request and/or Sale
    Replies: 5
    Last Post: 06-24-2009, 12:35 AM
  2. Project Explorabot - Roving wireless camera bot.
    By Pinter75 in forum Project Showcase
    Replies: 4
    Last Post: 11-14-2008, 09:40 PM
  3. Pan and Tilt Camera Kit
    By kanan in forum Robotics General Discussion
    Replies: 1
    Last Post: 09-21-2008, 09:47 PM
  4. Question(s) Pan and Tilt Kit Interface
    By sunjava in forum Software and Programming
    Replies: 5
    Last Post: 08-18-2008, 11:32 PM
  5. Project Wii nunchuck + Arduino controlling a Pan and Tilt Camera
    By Alex in forum Robotics General Discussion
    Replies: 15
    Last Post: 04-29-2008, 10:06 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •