Page 1 of 2 12 LastLast
Results 1 to 10 of 15

Thread: Dream Servo

  1. #1
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    128

    Dream Servo

    Ok, we've had lots of discussions over the past few days about servos, both serial and PWM. There's clearly a ton of servos out there, but we never seem to be happy about them! We got into a discussion about this here on campus, but of course the people on this board have a lot more experience than the noobs in my lab. I'm wondering what "your dream servo" would be? What sort of size, features, etc would you want?

    -Fergs

  2. #2
    Join Date
    Jul 2008
    Location
    Belgium
    Posts
    633
    Images
    2
    Rep Power
    62

    Re: Dream Servo

    Personally, I'd go for an AX-12+ style servo, as in maximum size constraints. Higher torque would be nice, RX-64-ish or so.

    Firmware-wise I'd like to see internal S-curve calculation, and a decent load indication.
    Ability for a multi-master bus would be nice too, or at least a way to alert the master that there's an issue with the servo, or when it's reached it's position or so. Then again, if it's a multi-master system, you could build a snake bot with nothing but servo's (token passing)

    Due to some recent brainstorms, I'd also like the ability to set the servo's position according to an analog voltage. Eg. 0v = 0°; 5v = 90°. That'd make for some interesting analog robots.. although it's not too hard to do in analog hardware, the amount of chips piles up fast.
    Artificial Intelligence is no match for Natural Stupidity

    "For a list of all the ways technology has failed to improve life, press three" - Alice Kahn

    Resistance is futile! (if < 1)

  3. #3
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Dream Servo

    The RX-64 for $25. Done.
    I Void Warranties´┐Ż

  4. #4
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: Dream Servo

    Personally I really think Robotis is on the right track, only thing that could be improved is the cost.

    I'd love to see an AX-12 that was compatible with the RX/DX series RS485 as well, maybe with a built in voltage reg.

  5. #5

    Re: Dream Servo

    Robotis type, with 360 deg. positioning feedback encoder-style. And interchangable gearboxes that fit right to the servo horn and face (like the ServoCity models). This would allow simple choice of speed vrs. torque. As long as we are talking ultimate lets also have a full bearing opposite the servo horn. I think that right now the AX-12 is a good value for the money. The gearboxes wouldn't be that expensive if they were built in quantity.

  6. #6

    Re: Dream Servo

    DC Robotic has a great idea with interchangeable gear boxes. I think that walkers need lower speed and higher torque than many other servo applications, for example. The ServoCity models are very large, however. The gearbox interchangeablility needs to be designed into the servo system and not an after-market item.

    I'd be very happy with a less expensive version of the RX-64 having a beefier gearbox, lower gear ratio, and a slower speed than the existing device.

  7. #7
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Dream Servo

    The funny thing about super-low gear ratios - they're kinda hard to squeeze into a standard size case and keep them from exploding, unless you build them from unobtanium...
    I Void Warranties´┐Ż

  8. #8
    Join Date
    Jul 2008
    Location
    Belgium
    Posts
    633
    Images
    2
    Rep Power
    62

    Re: Dream Servo

    good point.

    I would like to correct: I'd like an AX12 sized servo with a built-in hydraulic system instead of just a dc motor. No sugar with that please.

    Incidentally: does anyone know of the AX12 FW being available anywhere? I don't mean the hex files, but the actual code.
    Artificial Intelligence is no match for Natural Stupidity

    "For a list of all the ways technology has failed to improve life, press three" - Alice Kahn

    Resistance is futile! (if < 1)

  9. #9
    Join Date
    Feb 2009
    Location
    Mesa, AZ
    Posts
    351
    Images
    84
    Rep Power
    49

    Re: Dream Servo

    Quote Originally Posted by Adrenalynn View Post
    The RX-64 for $25. Done.
    In a perfectly symmetrical square case(not cube) with the shaft centrally located.

  10. #10
    Join Date
    Apr 2009
    Location
    Brisbane, Australia
    Posts
    48
    Rep Power
    37

    Re: Dream Servo

    My dream servo would have a reasonably high torque, good linearity, strong gearbox and decent cost.

    But, manny's suggestions for a square servo is not bad either.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. RC & Serial Servo Controller Kit
    By Al1970 in forum Garage Sale
    Replies: 0
    Last Post: 01-10-2009, 12:39 AM
  2. Question(s) servo and motor controllers
    By csdude in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 06-15-2008, 08:23 PM
  3. Question(s) Phidgets and servo voltage
    By Eric in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 05-12-2008, 08:32 AM
  4. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM
  5. Programming a Continious Rot Servo
    By Sirstrafe in forum Software and Programming
    Replies: 3
    Last Post: 04-27-2007, 09:11 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •