Results 1 to 10 of 10

Thread: climbing robots

  1. #1
    Join Date
    Jul 2009
    Location
    mumbai,maharashtra,india
    Posts
    25
    Rep Power
    31

    climbing robots

    does anyone hav idea fr making a wall climbimg robot(surface is smooth and has high traction,so more easy).links will be a welcome.wat to use fr sticking the bot to the wall and frm where can i get it?????????????????????

  2. #2

    Re: climbing robots

    [ame="http://www.youtube.com/watch?v=ECpY2N5rgcM"]YouTube - Gecko Robot[/ame]


    Stanford Uni had some special material developed for that little buggers feet iirc google "stanford gecko robot" and you should be able to find some better info though.

  3. #3
    Join Date
    Jul 2009
    Location
    mumbai,maharashtra,india
    Posts
    25
    Rep Power
    31

    Re: climbing robots

    thnx fr helping but the robot is too hard for me . i am now thinking of something that would act like a tape -as force is aplied it will get removed and it will easily stick to the wall and it will be attched to the wheels .can anyone tell me any substance which is eligible for this task.90 degree climb with around 10 to 15 feet .can u tell the adhesive to use and good motor with high torque.

  4. #4
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    174

    Re: climbing robots

    I would google around, contact manufacturers, and buy a few hundred samples. Then I would test and retest them at various temperature and humidity ranges in the desired operating range. I would also keep them exposed over time to see if they dry out.

    Most wall climbers in the hobby space use a vacuum action, like an inverse hovercraft.
    I Void Warranties´┐Ż

  5. #5
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    71

    Re: climbing robots

    There has been some research on using Van Der Waals force to work the same way a Gecko does on a wall. I believe carbon nano-tubes were used for the prototype. I think that is how the one in the video works.
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  6. #6
    Join Date
    Jul 2008
    Location
    Belgium
    Posts
    633
    Images
    2
    Rep Power
    59

    Re: climbing robots

    Not too easy to make by yourself though.
    I've seen it done by making a mold in a laser engraver, making tiny dots in a plastic, and then casting silicone rubber into it.

    Wasn't too efficient though..
    Artificial Intelligence is no match for Natural Stupidity

    "For a list of all the ways technology has failed to improve life, press three" - Alice Kahn

    Resistance is futile! (if < 1)

  7. #7

    Re: climbing robots

    What [ame="http://www.youtube.com/watch?v=U7dS-VSKlxM"]Lynn said[/ame]. (The second part.)

  8. #8

    Re: climbing robots

    Awesome post robologist! I didn't think that suction on that scale was possible interesting find!

  9. #9
    Join Date
    Jul 2009
    Location
    mumbai,maharashtra,india
    Posts
    25
    Rep Power
    31

    Re: climbing robots

    thnx robologist fr the awesome and inspiring video

  10. Re: climbing robots

    Hi. A wall climbing robot called as TBCP II was developed by the researchers of Simon Fraser University at Burnaby from the inspiration of gecko. It uses PDMS (Polydimethylsiloxane) as an adhesive material. It can climb vertical surfaces easily. Moreover, it can move over the inside and outside corners. You can catch more details and a video of it in the below link.

    http://www.roboticsbible.com/tbcp2-w...ing-robot.html

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  2. sony robots
    By openmindedjjj in forum Robotics General Discussion
    Replies: 6
    Last Post: 10-10-2008, 09:30 AM
  3. Interesting Robots at SIGGRAPH 2008
    By metaform3d in forum Robotics General Discussion
    Replies: 3
    Last Post: 08-13-2008, 10:23 AM
  4. Project Really Small Robots (RSRs)
    By LinuxGuy in forum Rovers
    Replies: 51
    Last Post: 08-07-2008, 12:24 PM
  5. robots who learn. what happened to them..
    By openmindedjjj in forum Robotics General Discussion
    Replies: 36
    Last Post: 07-02-2008, 03:46 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •