Page 3 of 3 FirstFirst 123
Results 21 to 30 of 30

Thread: Pic servo control question

  1. #21

    Re: Pic servo control question

    You can download a servo driver for the Propeller on the object exchange.
    http://obex.parallax.com/

    It takes up one cog. That way you don't need any extra hardware.

  2. Re: Pic servo control question

    Yeah, but it was my intent to save on propeller memory. Riding at 30mph it will already have a load of work to do to keep itself from wrecking.

  3. #23

    Re: Pic servo control question

    Each of the 8 COGs are deterministic at 20MIPS each or 160MIPS in total. The servo driver executes in a single COG and can control 32 servos. Very little HUB memory is needed. At 30mph that's 37,878 instructions per inch per COG.

  4. Re: Pic servo control question

    Yeah, well, it's a battle you're not going to win. When I get all I want I will be working with:
    1 or 2 ir heat sensors
    gps
    3 sonar sensors
    many front bumper ir sensors
    break motor
    steering motor
    servos for each sonar sensor
    2 servos for the engine
    rpm measurement from the engine
    actual rpm of shaft after leaving clutch to detect slippage
    accelerometer
    compass
    sd card writing/reading
    emergency warning leds
    cmu cam
    rf transmitter/receiver
    -and a lot more once I have all this
    Some people have already tried telling me I won't have a space problem, but trust me, I will.

  5. #25
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    128

    Re: Pic servo control question

    Ok, now I have to ask: What exactly do you intend to do with a CMUCam on a bot moving 30mph?

    -Fergs

  6. #26

    Re: Pic servo control question

    Wow so adding 2 servos pushed the Propeller memory over the edge. Still very impressive that you're controlling all those devices with a Prop.

  7. Re: Pic servo control question

    I was hoping to spread out the use, give me more time for calculations and such. Also, I'm currently not doing all that with the prop. I only have the hardware for 1/3 of it and I'll buy the rest in the next couple weeks. My robot isn't quite done either, but after doing some welding on the steering system yesturday I'm ready to test it out. If all works, it will be autonomous without breaks, which I will finish up in a week or two. Then it's the harder part of getting my 1/3 hp 12v motor hooked up so I can go backwards with the bot, then the hardest pard will be the alternator because I have to modify the engine shaft as well as mount the alternator in a way that it can tighten the belt easily. I'm also not sure how to run it, I'll probably end up wandering around some junkyard looking for a battery charger I can connect to it.

  8. Re: Pic servo control question

    Here is a pic of what I'm doing this for. I'll post a thread specifically on this later once I get bit more done on it.

  9. #29
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Pic servo control question

    Cool chassis! Looks like it'd be interesting for a Magellan-type application.

    Now, if you could control one of those Llamas with a PIC, that'd ROCK!
    I Void Warranties´┐Ż

  10. Re: Pic servo control question

    Idk about controlling them, but I did think about chasing them
    As for the chassis it really isn't all that great. After many weeks of working on it it still came out with a lot of problems. I think I've done a good job covering them up and fixing them though. I've definitely learned a great deal about mechanics and welding while building it, and now its time to do the same with it's software.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Servo Control Circut
    By WarriorofHonour in forum DYNAMIXEL & Robot Actuators
    Replies: 9
    Last Post: 06-04-2009, 12:06 AM
  2. Disaster! Video of phidget servo control (Comedy included!)
    By Semicton in forum Software and Programming
    Replies: 6
    Last Post: 02-22-2009, 02:08 AM
  3. RC & Serial Servo Controller Kit
    By Al1970 in forum Garage Sale
    Replies: 0
    Last Post: 01-10-2009, 12:39 AM
  4. Question(s) Servo control using FSRs
    By heat in forum Arbotix, Microcontrollers, Arduino
    Replies: 15
    Last Post: 01-05-2009, 03:32 PM
  5. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •