Page 1 of 2 12 LastLast
Results 1 to 10 of 12

Thread: Introducing the Mech Warfare Hexapod League

  1. #1
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    139

    Introducing the Mech Warfare Hexapod League

    Hey guys!

    This is an idea that I've been tossing around for a bit, and really, I can't see any reason why not to go this route. I've decided we're going to open up a Hexapod League for Mech Warfare, to hopefully tap into the crowd that already owns hexapods (myself included). It will be an easy transition to a Mech Warfare ready bot with these platforms, as their payload is significantly higher than that of a quad or biped.

    Now, because of these hefty payload advantages as well as increased mobility, Hexapods are going to be in a separate league for the ranked matches. Exhibition matches are of course 'whatever goes' but for the ladder itself, it would be too difficult to balance hexapods vs quads/bipeds.

    Hexapods will essentially have the same exact rule set as that of a quadrapod. 4 target panels, etc, however given their design I think it is prudent that target panels be mounted on the turret itself, otherwise we run into the risk of the legs at least partially concealing them.

    Anyway, I hope this opens the door to more competitors! Can't wait to see what some people come up with in terms of designs.

    I'll have updated rules posted in the near future, just throwing this out there for discussion for the time being.

  2. #2
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    78

    Re: Introducing the Mech Warfare Hexapod League

    Hi,

    Sounds like an great idea!
    I saw your thread for about 30 min ago and have been thinking about a very different design for a Mech inspired hexapod, but I'm not sure if I'm able to get all the way from Norway to the Robogames. Would be cool though. There should be some good plattforms in the marked for a Mech-Hex. Their ability to move fast (and stable) in all directions combined with IK body movements and a rotating turret would be cool. One feature that would be awesome to try is a combination of sideways walking in an arc and a rotating turret that keep the weapons on the spot all the time. Hitting a moving target should be much harder.

    Anyway, i hope to see some of Phoenix's modified sisters out there

    -Zenta

  3. #3

    Re: Introducing the Mech Warfare Hexapod League

    Yeah! Hex-Mechs! That'll be fun! Some thoughts though...

    Quote Originally Posted by Tyberius View Post
    Hexapods will essentially have the same exact rule set as that of a quadrapod. 4 target panels, etc, however given their design I think it is prudent that target panels be mounted on the turret itself, otherwise we run into the risk of the legs at least partially concealing them.
    [1] Where are you going to mount the turret target plate if there IS no turret? Like someone somehow managed to put their guns on the front of the mech?

    [2] I can't quite visualize the legs partially concealing target plates. I mean, won't there be a target plate for each and every leg?

    Just thinking.
    Last edited by MSK Mech Commander; 08-04-2009 at 02:24 PM. Reason: Revision

  4. #4
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    139

    Re: Introducing the Mech Warfare Hexapod League

    Due to technical constraints we're sticking with 4 target panels total, even for Hex-Mechs.

    The target plate mounting is just a suggestion, obviously common sense and fairplay will be a factor here. If they can be mounted on the outer 4 legs without constricting movement, fine by me.

  5. #5

    Re: Introducing the Mech Warfare Hexapod League

    Cool, good to know.

  6. #6
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    78

    Re: Introducing the Mech Warfare Hexapod League

    Check out this cool animated hexapod:



    -to be inspired from when designing your own Hex-Mech.
    Another cool video of the same hex:



    Something like that would be awesome!

    -Zenta

  7. Re: Introducing the Mech Warfare Hexapod League

    Excellent idea, especially for those of us just getting into the hobby.
    Prae

  8. #8

    Re: Introducing the Mech Warfare Hexapod League

    Maybe like Mechadon http://homepage.mac.com/roninsfx/Tea...Theater16.html

    [ame="http://www.youtube.com/watch?v=El8ne4zSCY0"]YouTube - Rammstein vs Mechadon[/ame]

  9. Re: Introducing the Mech Warfare Hexapod League

    Great idea. Although I am based in the UK.

    Are there any UK hexapod/Quad owners that would be interested in a local UK based Hexapod/Quad League?

    Infact I live quite close to an international airport with regular
    (& cheap) flights to most of Europe - so it could even become a
    European league.

  10. #10

    Re: Introducing the Mech Warfare Hexapod League

    Quote Originally Posted by Tyberius View Post
    Now, because of these hefty payload advantages as well as increased mobility, Hexapods are going to be in a separate league for the ranked matches. Exhibition matches are of course 'whatever goes' but for the ladder itself, it would be too difficult to balance hexapods vs quads/bipeds.

    Hexapods will essentially have the same exact rule set as that of a quadrapod. 4 target panels, etc, however given their design I think it is prudent that target panels be mounted on the turret itself, otherwise we run into the risk of the legs at least partially concealing them.
    Just for clarification, the Hex-Mechs will be under the same rules as the Airsoft League, right?

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Mech Warfare 2010 Draft Rules
    By lnxfergy in forum Mech Warfare
    Replies: 125
    Last Post: 05-24-2010, 12:47 PM
  2. Mech Warfare FAQ- Please Read if Participating.
    By DresnerRobotics in forum Mech Warfare
    Replies: 1
    Last Post: 07-29-2009, 12:44 PM
  3. Mech Warfare Rules and Guidelines
    By DresnerRobotics in forum Mech Warfare
    Replies: 238
    Last Post: 07-29-2009, 12:43 PM
  4. Replies: 12
    Last Post: 06-02-2009, 12:47 PM
  5. Entry-level Mech Warfare
    By imagitronics in forum Mech Warfare
    Replies: 4
    Last Post: 02-17-2009, 08:46 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •