Results 1 to 4 of 4

Thread: Timer for Servo or Motor for cigarette dispenser?

  1. Timer for Servo or Motor for cigarette dispenser?

    I'm trying to build a simple little box that unlocks every 3 hours.

    I am thinking of a servo or motor to use as the unlocking mechanism.

    I don't want to hook it up to a computer. What kind of circuit could I have to run this?

    What about power?

    Any ideas?

    What is this for? Its kinda embarassing... i'm trying to quit smoking and I want to make a cigaretter dispenser so i can gradually cut back.

    Thanks so much! Really need this.


  2. #2

    Smile Re: Timer for Servo or Motor for cigarette dispenser?

    Nothing to be embarrassed about, I think it's a brillant idea! First of all I don't have a suggestion for servo/controller, I don't know enough about that sort of thing, sorry. But I am proud to say that I'm now a non smoker, after more years of being a smoker than not so I feel your pain and appreciate your effort in trying something new. What I can suggest is to look into something in the market similar to what you are looking for. There are medicine pill dispensers with alarms that may be big enough. However I'm not sure if they make them unlockable via the timer. And being an ex smoker I understand the need for a locking system, if nothing it's a good mental barrier anyway it just seems like something like this should be in the market, try surfing something up before trying to make one? In my experience it's almost always more costly to try and make something than to buy one designed already.... But it's always more fun to "make" stuff though, so I'm not trying to talk you out of that. The fact that you're lookin into this is a big step and I wish you luck!

    -crabfu

  3. #3
    Join Date
    Feb 2009
    Location
    Mesa, AZ
    Posts
    351
    Images
    84
    Rep Power
    49

    Re: Timer for Servo or Motor for cigarette dispenser?

    How about gutting a digital alarm clock and rigging something to the speaker output? Maybe use this as a Hi/Lo signal to trigger a servo opening? Or maybe wire the speaker leads to a solenoid actuated locking mechanism? No computer required, and the bonus is you gain battery backup in case of power outage! Of course you have to reset the alarm every three hours.

    And good luck! I'm two months smoke-free myself but its still a daily battle.
    Last edited by mannyr7; 08-05-2009 at 11:38 PM.

  4. #4
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    176

    Re: Timer for Servo or Motor for cigarette dispenser?

    I think the RTC (Real Time Clock) is your challenge. I wouldn't approach the challenge without a decent microcontroller and RTC. I'm actually in the process of interfacing a M41T56C64 real time clock chip to an Arduino...
    I Void Warranties´┐Ż

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. C# Help
    By metaform3d in forum Software and Programming
    Replies: 11
    Last Post: 04-21-2008, 10:08 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •