Results 1 to 6 of 6

Thread: Videos of Firgelli L12 Actuators needed

  1. Videos of Firgelli L12 Actuators needed

    Hi,

    I am looking for videos of the Firgelli L12 actuators with 100mm using 12 Volts under zero load.

    there are three gearing options
    1) 1:50
    2) 1:100
    3) 1:210

    Does anyone have a video showing the speed of these actuators?
    it would be very helpful in choosing which to go with

    thanks

  2. #2

    Re: Videos of Firgelli L12 Actuators needed

    Don't know which ratio it is, but imagine Firgelli could tell you.

    [ame="http://www.youtube.com/watch?v=jIsIWzzmd9U"]YouTube - L12 FIRGELLI TECHNOLOGIES MINI LINEAR ACTUATOR[/ame]

  3. #3
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    173

    Re: Videos of Firgelli L12 Actuators needed

    Remember that that's no-load speed too...
    I Void Warranties´┐Ż

  4. Re: Videos of Firgelli L12 Actuators needed

    Thanks!

    I have seen those but like you said there were no specs on it..thats why i posted here

    Firgelli is on vacation for 2 weeks so there is noone there....

    could someone post on this forum those three actuators?

    thanks

    dave

  5. #5
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: Videos of Firgelli L12 Actuators needed

    Quote Originally Posted by badboi View Post
    Thanks!

    I have seen those but like you said there were no specs on it..thats why i posted here

    Firgelli is on vacation for 2 weeks so there is noone there....

    could someone post on this forum those three actuators?

    thanks

    dave
    I'm not sure I've actually seen any of our regular visitors actually using these in a project. Further, I doubt anyone out there has all 3, or even more than one style. Do they give the raw RPM of the motor under load? I'd think that a straight out calculation would be more useful than videos of unknown loads/inconsistent setups...

    -Fergs

  6. #6
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    173

    Re: Videos of Firgelli L12 Actuators needed

    Ooops has one, but I've no idea which. I agree, the no-load setup doesn't mean anything at all in the real world.
    I Void Warranties´┐Ż

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Firgelli L12 versus Hitec 5990TG
    By Vsions in forum DYNAMIXEL & Robot Actuators
    Replies: 27
    Last Post: 12-23-2008, 02:22 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •