Page 1 of 5 12345 LastLast
Results 1 to 10 of 49

Thread: Autonomous robot's navigation

  1. #1

    Autonomous robot's navigation

    Hello,

    Now I work at associative video memory. The method still in developing (now it version 0.5)
    but it gives good results already today.

    I am dealing with research of computer vision in parallel with my main job
    at "Impulse" more than three years (it is my hobby).

    About me: http://edv-detail.narod.ru/EDV_resume.html

    In the beginning my achievements were insignificant and little part of ideas has worked properly.
    But I did not surrender. I generated big quantity of hypotheses and then test it.

    The most ideas did not work indeed but those that worked were similar to particles of gold
    in huge quantity of dross. My associative video memory method is working indeed.

    ============================- Common information -==========================

    Algorithm AVM uses a principle of multilevel decomposition of recognition matrices,
    it is steady against noise of the camera and well scaled, simply and quickly
    for training, also it shows acceptable quick-action on a greater image resolution
    of entrance video (960x720 and more). The algorithm works with grayscale images.

    The detailed information about AVM algorithm can be looked here:
    http://edv-detail.narod.ru/AVM_main.html

    AVM SDK v0.5 with examples of using and tests for comparison
    of characteristics of the previous and new versions:
    http://edv-detail.narod.ru/AVM_SDK_v0-5.zip

    Demonstration video how to train AVM:
    http://edv-detail.narod.ru/Face_training_demo.avi

    AVM demo with the user interface (GUI), installation for Windows:
    http://edv-detail.narod.ru/Recognition.zip

    Connect the web-camera and start AVM demo after installation of "Recognition.exe".
    After starting the program will inform that there is not stored previously data
    of training AVM and then will propose to establish the key size of the image
    for creation of new copy AVM. Further train AVM using as an example Face_training_demo.avi.

    ========================- Robot's navigation -=========================

    I also want to introduce my first experience in robot's navigation powered by AVM.

    Briefly, the navigation algorithm do attempts to align position of a tower
    and the body of robot on the center of the first recognized object in the list
    of tracking and if the object is far will come nearer and if it is too close it
    will be rolled away back.

    See video below:



    I have made changes in algorithm of the robot's control (Navigator.cpp)
    also I have used low resolution of entrance images 320x240 pixels.
    And it gave good result (see "Follow me"):



    Source code of "Navigator" program:
    http://edv-detail.narod.ru/Navigator_src.zip

    During experiments I noted significant reserve of quick-action
    when AVM v0.5 is working with resolution 320x240.

    And it give me good conditions for starting of new experiments
    in navigation field (algorithm "Location tree"), of course I also
    will try to make AVM faster with resolution 640x480 in the future.

    Also I finished some experiments with "Natural beacons":


    Source code of demo (project "Beacons test"):
    http://edv-detail.narod.ru/Navigator_Tool_Kit.zip

    I hope that this information can help you in questions:
    How we can use AVM algorithm?

    If somebody can read in Russian then welcome: (Russian thread: "Autonomous robot's navigation").

  2. #2
    Join Date
    Dec 2008
    Location
    Washington
    Posts
    312
    Images
    35
    Rep Power
    41

    Re: Autonomous robot's navigation

    Wow this works great so far! How easy would it be to interface it with python?
    Dalton Caughell

  3. #3

    Re: Autonomous robot's navigation

    WOW Nice I'll be taking a more indepth look at this over the weekend

  4. #4
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Autonomous robot's navigation

    Dear Dmitriy, first - welcome to the Trossen Robotics Forum!

    Thank you most sincerely for sharing such a comprehensive result of your investigations into computer vision/recognition and vision-based navigation. A tremendous amount of information to absorb here - digital video is my specialty - and I look forward to learning from your explorations and documentation.

    I do hope you will find yourself visiting us regularly!

    In response to questions about "ease of integration" - this is a research project, and its intent is to advance a field and body of knowledge. IMHO: If that's the first question that comes to mind, this probably isn't the best place to start.
    I Void Warranties�

  5. #5

    Re: Autonomous robot's navigation

    Quote Originally Posted by ROBOTMAN View Post
    Wow this works great so far! How easy would it be to interface it with python?
    I don't plan a development of the interface for python at the moment but it is possible in the future.

    But AVM v0.5 SDK with examples of using is available.

    The compilation is possible by one of compiler:
    AVM_SDK\samples\vc6.prj\AVM_prj.dsw for Microsoft Visual C++ 6.0
    AVM_SDK\samples\vc9.prj\AVM_prj.sln for Microsoft Visual Studio 2008
    Also library OpenCV_1.0 is needed for compilation.

    The algorithm "Associative video memory" is commercial project but you can use AVM SDK in your researches and in non-commercial projects.

    I will try to prepare the detailed documentation about using of AVM v0.5 SDK.

    Also I will share with you results of my future researches in robot's navigation.
    Last edited by EDV; 08-28-2009 at 03:07 AM.

  6. #6
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Autonomous robot's navigation

    Congrats too on spinning AVM off into a commercial project!
    I Void Warranties�

  7. #7

    Re: Autonomous robot's navigation

    Source code of "Navigator" program and "Navigator tool kit" was prepared for Russian community (some comments in source code in Russian).

    But if you would show interest to this topic then I could adapt it to English community too.

  8. #8
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Autonomous robot's navigation

    [Mod Note: Thread-Jack Relocation: http://forums.trossenrobotics.com/showthread.php?t=3600 Nikhil Thiruvengadam's mower project moved]
    I Void Warranties�

  9. #9

    Re: Autonomous robot's navigation

    Awesome! I can't read russian "directly", but Google is pretty useful

  10. #10

    Re: Autonomous robot's navigation

    Robot navigation by gate from point "A" to "B"





    First an user must set the visual beacons (gates) that will show direction where robot has to go.
    Robot will walk from gate to gate. If the robot recognize "target" then he come nearer and stop walking.

    Navigation application (installation for Windows):
    http://edv-detail.narod.ru/Recognition.zip

    Installation also contains source code of robot control driver (InstDir\RobotController_src).
    So you can adapt it to your robots and repeat my navigation experiments by yourself.


    Also available source code of navigation application (but all comments in Russian):
    http://edv-detail.narod.ru/Navigator_src.zip

Thread Information

Users Browsing this Thread

There are currently 4 users browsing this thread. (0 members and 4 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  2. on encouraging autonomous mechs
    By societyofrobots in forum Mech Warfare
    Replies: 116
    Last Post: 11-23-2009, 11:25 AM
  3. Ideas for Autonomous Kondo Robots
    By Atom in forum Humanoids, Walkers & Crawlers
    Replies: 8
    Last Post: 08-23-2008, 07:45 PM
  4. Discussion What is a "robot"????
    By Matt in forum Robotics General Discussion
    Replies: 83
    Last Post: 07-22-2008, 09:22 AM
  5. robots who learn. what happened to them..
    By openmindedjjj in forum Robotics General Discussion
    Replies: 36
    Last Post: 07-02-2008, 03:46 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •