Page 4 of 5 FirstFirst 12345 LastLast
Results 31 to 40 of 49

Thread: Autonomous robot's navigation

  1. #31

    Re: Autonomous robot's navigation

    It is a testing of odometry-localization algorithm at Simpsons map. The Quake 3 mod was used as environment emulator for capture of live video by AVM Navigator v0.7 in this test.




    Simpsons map for Quake 3


  2. #32

    Re: Autonomous robot's navigation

    It is first simple test of new version AVM Navigator v0.7 in mode "Navigation by map".


  3. Re: Autonomous robot's navigation

    Hi Dmitri and to all trossenrobotics forum members. I want to share with you Argon Technology's designed world first, fully autonomous robotic at Fusion and TGA laboratory.

  4. #34

    Re: Autonomous robot's navigation

    2artash:
    And how this solution touched "computer vision" and "robot navigation" problems?

  5. #35

    Re: Autonomous robot's navigation

    It is experiment of autonomous robot's navigation by map in emulation mode. Primarily robot plans the path from current location to the target position (big green circle) and then robot begins walking to the interim point of path (big red circle). When interim point is achieved then robot gets direction to the other point and so further until finish of path.

    Last edited by EDV; 04-23-2011 at 05:57 AM.

  6. #36
    Join Date
    Feb 2009
    Location
    Mesa, AZ
    Posts
    351
    Images
    84
    Rep Power
    53

    Re: Autonomous robot's navigation

    Quote Originally Posted by EDV View Post
    It is experiment of autonomous robot's navigation by map in emulation mode. Primarily robot plans the path from current location to the target position (big green circle) and then robot begins walking to the interim point of path (big red circle). When interim point is achieved then robot gets direction to the other point and so further until finish of path.
    Waypoints is the term you are speaking of. Excellent work!

  7. #37

    Re: Autonomous robot's navigation

    Thank you, I will keep in mind (path points = waypoints)

  8. #38

    Re: Autonomous robot's navigation

    So, let's continue with waypoints in real environment
    Turn is passed in autonomous "Navigation by map" mode by real robot.

    Last edited by EDV; 04-25-2011 at 01:58 PM.

  9. #39

    Re: Autonomous robot's navigation

    Autonomous walking of robot from bedroom to another room based on visual landmark navigation (AVM Navigator v0.7).


  10. #40

    Re: Autonomous robot's navigation

    AVM Navigator v0.7 will be released soon.
    In new version will be added two modes: "Marker mode" and "Navigate by map".

    Marker mode



    Marker mode provides a forming of navigation map that will be made automatically by space marking. You just should manually lead the robot along some path and repeat it several times for good map detailing.

    Navigation by map



    In this mode you should point the target position at the navigation map and further the robot plans the path (maze solving) from current location to the target position (big green circle) and then robot begins automatically walking to the target position.



    For external control of "Navigate by map" mode will be added new module variables:

    NV_LOCATION_X - current location X coordinate;
    NV_LOCATION_Y - current location Y coordinate;
    NV_LOCATION_ANGLE - horizontal angle of robot in current location (in radians);


    Target position at the navigation map
    NV_IN_TRG_POS_X - target position X coordinate;
    NV_IN_TRG_POS_Y - target position Y coordinate;

    NV_IN_SUBMIT_POS - submitting of target position (value should be set 0 -> 1 for action).

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  2. on encouraging autonomous mechs
    By societyofrobots in forum Mech Warfare
    Replies: 116
    Last Post: 11-23-2009, 11:25 AM
  3. Ideas for Autonomous Kondo Robots
    By Atom in forum Humanoids, Walkers & Crawlers
    Replies: 8
    Last Post: 08-23-2008, 07:45 PM
  4. Discussion What is a "robot"????
    By Matt in forum Robotics General Discussion
    Replies: 83
    Last Post: 07-22-2008, 09:22 AM
  5. robots who learn. what happened to them..
    By openmindedjjj in forum Robotics General Discussion
    Replies: 36
    Last Post: 07-02-2008, 03:46 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •