Page 1 of 6 12345 ... LastLast
Results 1 to 10 of 54

Thread: The Ultimate Arbotix Thread

  1. #1
    Join Date
    Nov 2007
    Posts
    397
    Images
    71
    Rep Power
    49

    The Ultimate Arbotix Thread

    Hey everyone, I was one of the people that spent some time beta testing the Arbotix, and I thought it would be a good idea to start and "ultimate" thread for it. I have noticed that there are several people that have already bought an arbotix, and from the sound of things they are having a lot of fun with them. I personally think that this board is awesome, and cant wait to see what projects people come up with using it.





    I have been working on getting a mech ready for next year, but I haven't had much success with my previous designs. I got bored today and threw this bot together in a couple hours. I haven't had much time to do any walking or anything but I figured I could post a few little videos of what I have so far. Please excuse the fact that this thing looks like a mess, its not a very good layout and I hacked it together pretty fast. Hopefully I will have it looking a little better in a few weeks.




    Anyway, please post your thoughts on the arbotix, your questions, and at least a link to your arbotix based projects on here. Above all keep building!
    Last edited by sthmck; 10-18-2009 at 11:02 PM.

  2. Re: The Ultimate Arbotix Thread

    Looks nice man!
    and woo, im one of those people that have a arbotix, ill post some videos soon (atm kinda busy with 'real life matters')

  3. #3
    Join Date
    Nov 2007
    Posts
    397
    Images
    71
    Rep Power
    49

    Re: The Ultimate Arbotix Thread

    I just got a chance to work on my mech over the weekend, I changed a few things up as far as the leg design goes. What I really wanted everyone to see was some poses being exported to the board, as well as using some of the boards IO. I basically have three ir sensors hooked up and poses are triggered when and IR sensor detects something in front of it. For some stupid reason I was having trouble getting the poses exported properly but after a little sleep my brain started working better and I got things going.


  4. #4
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: The Ultimate Arbotix Thread

    I just sent a PM response about the protocol used by PyPose, and how to connect using a custom application, so I figured I would copy my response here for all to learn from:

    All of our programs are open source. If you have the PyPose program -- you already have the source. Python is just a scripting langauge, open PyPose.py or any of the .py files in a text editor and you'll see. (alternatively, you can browse the source on arbotix.googlecode.com, click on Source tab).

    The TEST command is basically our in-house way of checking out an ArbotiX before shipping it. To trigger it, send out:
    0xff 0xff 253 2 25 231

    The protocol is the same as talking to an AX-12 itself (basically, the PyPose sketch acts as a bus pass through, or, given special instructions, it executes commands). The first two 0xff are the header for the packets (just like an AX-12 would recieve). The 253 is the ID, your servos are IDs 1-X, 253 tells the arbotiX this packet SHOULD NOT be passed through, and that it instead should interpret the packet itself. 25 is the instruction (arbotiX test or ARB_TEST). The 2 is the length of the packet (see the AX-12 datasheet or the PyPose.py source for details, but general format = # of parameters + 2, test takes no parameters). The 231 is a checksum (255 - ((id + length +instruction + any parameters)%256)). All of the other special arbotiX commands, such as loading a sequence, loading the poses that are part of a sequence, or playing it, follow this format.
    Also, for fun, here's a quick video of early work on my Salamander-inspired walker, Sally:


    -Fergs
    Last edited by lnxfergy; 11-08-2009 at 03:48 PM. Reason: helps when you do the checksum calculation correctly

  5. Re: The Ultimate Arbotix Thread

    Hey man, Sally looks very nice, cool gait too, show us more! (also, if i may ask, can you currently show anything from NUKE yet? i'd love to see how that goes, did you use it for sally?)
    Last edited by Suicidal.Banana; 11-09-2009 at 07:55 AM.

  6. #6
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: The Ultimate Arbotix Thread

    Quote Originally Posted by Suicidal.Banana View Post
    Hey man, Sally looks very nice, cool gait too, show us more! (also, if i may ask, can you currently show anything from NUKE yet? i'd love to see how that goes, did you use it for sally?)
    That's all there is to show right now -- Sally just got up and running. It's all pose and caputre (6 poses for that forward walk). I'm actually not certain at this time if there IS a closed form solution to the IK for Sally. There's a few issues that need to be worked out before continuing with the bot, those Lynxmotion tubes are shaking themselves loose as the bot walks and I'll need to do some serious weight distribution work to get it to walk on surfaces like carpet.

    As for NUKE, there is an image of the GUI in the PyPose documentation. The program is basically converging from two ends: there's the GUI that's mostly done, and there is the actual IK and gait generating code which is also mostly done, and then in the middle is the meshing of the two -- which is where most work is now needed.

    -Fergs

  7. Re: The Ultimate Arbotix Thread

    Okay thanks for the info on PyPose/NUKE, good luck on that middle part (ye i recently ran into the gui pic, which caused me to ask about NUKE ) and nice job on achieving that walk with 'just' pose usage, 'props' man.

  8. #8
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: The Ultimate Arbotix Thread

    Sthmck and I got a chance to sit down and run the pre-alpha version of NUKE on his quad, Jeff, this weekend at the Canadian National Robot Games. In about 30 minutes we had a full IK solution customized to his bot, and a default gait. Since we only started about an hour before the competition, he didn't have time to get the sensors attached to the bot, so he used just dead reckoning -- here's the third and final run, with a time of about 49s, which took third place behind Issy and Roz, two other arbotiX/NUKE powered robots.



    -Fergs

  9. #9
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    173

    Re: The Ultimate Arbotix Thread

    Congrats to Sthmck - and the arbotiX team too!
    I Void Warranties´┐Ż

  10. #10
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: The Ultimate Arbotix Thread

    And here's Issy's video (more info in his thread):


Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Bioloid The Ultimate Bioloid Thread
    By tom_chang79 in forum Humanoids, Walkers & Crawlers
    Replies: 436
    Last Post: 09-22-2011, 12:27 PM
  2. The Ultimate Phoenix Thread
    By tom_chang79 in forum Humanoids, Walkers & Crawlers
    Replies: 126
    Last Post: 04-17-2011, 04:36 PM
  3. The Ultimate Axon Thread
    By Droid Works in forum Arbotix, Microcontrollers, Arduino
    Replies: 73
    Last Post: 10-21-2009, 11:21 PM
  4. Robonova The Ultimate Robonova Thread
    By engineer in forum Humanoids, Walkers & Crawlers
    Replies: 34
    Last Post: 06-15-2009, 02:15 PM
  5. Kondo 1HV The Ultimate KHR-1HV / 2HV Thread.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 20
    Last Post: 04-11-2009, 04:44 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •