Page 1 of 2 12 LastLast
Results 1 to 10 of 12

Thread: Bioloid Wireless Camera Set

  1. #1
    Join Date
    Sep 2008
    Location
    Albany NY area
    Posts
    22
    Rep Power
    40

    Bioloid Wireless Camera Set

    So I see at Robotis they are now selling the wireless camera set separately from the expert kit, but only "thru their distributors". Will that include Trossen? To be honest, the most interesting part for me would be the expert CD since I'm hoping there are some sources to the firmware on there that allows one to safely charge the battery. But I won't throw the camera away

    http://www.robotis-shop-en.com/shop/...php?number=679

    Camera-wise I'm thinking the surveyor blackfin is going to be more interesting. But I'm still trying to find appropriate vision software for Linux (esp. openembedded, but ubuntu in a pinch) that gets beyond the usual blob grouping.
    --
    Gorbag
    We are pattern matching machines

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Bioloid Wireless Camera Set

    You don't want to get within ten miles of that POS 2.4Ghz camera. But if you insist, I'll do you a MUCH better deal than that!

    Of course, you'll just end-up returning it, and I'll eat shipping. Never mind.

    The Blackfin camera is WiFi. Stick with that if you have that kinda money burning a hole in your pocket.

    As far as vision software goes, you can code whatever you want, sky's the limit, against OpenCV.
    I Void Warranties�

  3. #3
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: Bioloid Wireless Camera Set

    We will not be stocking this camera. If you have your heart set on it, we could arrange a special order with the next Robotis shipment we receive. That said, 'Lynn here offers very sound advice

  4. #4
    Join Date
    Sep 2008
    Location
    Albany NY area
    Posts
    22
    Rep Power
    40

    Re: Bioloid Wireless Camera Set

    @Adrenalynn: OpenCV - cool; I hadn't run across a pointer to that library before. Thanks! I've been looking at Lowe's SIFT algorithm (binary only windows, linux). But to get it to run under OE I have to reimplement it from the published papers. OpenCV may make that easier!

    @Tyberius: No worries. I like the blackfin much better; I only considered the Robotis camera for the software out of the expert kit. I'm not using the CM-5 much anyway so it's not worth the cost to me if the camera is really valueless.
    --
    Gorbag
    We are pattern matching machines

  5. #5
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Bioloid Wireless Camera Set

    NP - OpenCV is _the_ defacto-standard. It's slow, but it's rather very complete. And because it's such a standard, you'll findn umpteen examples on the Intarwebz, but also a good many complete book treatments if you search Amazon.
    I Void Warranties�

  6. #6
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    50

    Re: Bioloid Wireless Camera Set

    Quote Originally Posted by Adrenalynn View Post

    The Blackfin camera is WiFi. Stick with that if you have that kinda money burning a hole in your pocket.
    I've been considering the Blackfin with WiFi option for some time now. Can anyone here report what you have seen for frame rates at different resolutions over 802.11g? Say 160x128, 320x240 and 640x512? Also, how reliable has the connection been and up to what range (approximately)? Does the camera have auto-exposure capabilities that can be turned on and off? And finally(!) has anyone tried the 120 degree lens? I find the narrow FOV of most WiFi webcams to be a significant handicap when my robot is trying to track moving objects (using RoboRealm).

    Thanks!
    patrick

  7. #7
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Bioloid Wireless Camera Set

    >> I find the narrow FOV of most WiFi webcams to be a significant handicap when my robot is trying to track moving objects (using RoboRealm)

    Remember - the wider the lens, the fewer the number of pixels said moving object occupies - and therefore the harder it is to track them.
    I Void Warranties�

  8. #8
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    50

    Re: Bioloid Wireless Camera Set

    Quote Originally Posted by Adrenalynn View Post

    Remember - the wider the lens, the fewer the number of pixels said moving object occupies - and therefore the harder it is to track them.
    Good point! The trouble I have with the narrower FOV cameras is that a moving object can easily move out of the FOV before a tracking algorithm has time to catch up, especially if the frame rate is not very high.

    --patrick

  9. #9
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Bioloid Wireless Camera Set

    A typical lens/sensor on a webcam should see between 8'x6' @ 10ft and 6'x4.5' at 10ft.

    At even 15fps, it would need to be moving something along the lines of 60+ feet/sec not to at least get one frame. Around 41mph horizontally across the camera.

    How fast you can process that video is typically the question that needs to be addressed. If you shrink the number of available pixels down, you're going to have to do a lot more processing to recognize the object, so you kinda get a catch-22.

    That said - doing obstacle avoidance or looking for markers can be made a bunch easier with a wider lens, as long as the obstacles/markers are really large. Otherwise you pretty much are best suited with the stop-and-pan method, imho.
    I Void Warranties�

  10. #10
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    50

    Re: Bioloid Wireless Camera Set

    Great analysis! As it turns out, the object tracking I have done so far takes place much closer to the camera--more like 1-3 feet as shown in this video:

    http://www.pirobot.org/videos/0006/


    And if the object is already centered in the FOV, it can leave the FOV by moving just half of the width. Also, the object being tracked is usually something big and colorful so the object detection/recognition task is fairly easy. In practice, I found I had to use the fastest webcam I could find--the Philips SPC 1300NC at 90 fps--to get good tracking for quick object motion this close to camera.

    --patrick

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Replies: 128
    Last Post: 07-27-2012, 07:43 AM
  2. Bioloid The Ultimate Bioloid Thread
    By tom_chang79 in forum Humanoids, Walkers & Crawlers
    Replies: 436
    Last Post: 09-22-2011, 12:27 PM
  3. News/Announcement Want to win a Bioloid? Announcing the TRC Tutorial Contest!
    By DresnerRobotics in forum Project Showcase
    Replies: 28
    Last Post: 01-30-2010, 12:49 AM
  4. Project Motion sensor controlled Tilt and Pan Camera (wireless)
    By ACEX in forum Project Showcase
    Replies: 14
    Last Post: 07-08-2009, 03:55 AM
  5. Project Explorabot - Roving wireless camera bot.
    By Pinter75 in forum Project Showcase
    Replies: 4
    Last Post: 11-14-2008, 09:40 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •