Page 1 of 2 12 LastLast
Results 1 to 10 of 14

Thread: Powering my robot

  1. Powering my robot

    Hi,

    I'm new here, so thanks for having me. I'm from a programming background and have absolutely no idea when it comes to electronics. I'd like to build a robot consisting of the following:

    1 x VIA EPIA PX5000EG

    3 x Xbee Pro 60mW Series 1 with Wire Antenna connected to the VIA EPIA via 3 x XBee-Explorer-USB

    1 x PhidgetStepper Unipolar USB 4-Motor Stepper Controller connected to the VIA EPIA via USB and running 2 x Danaher 42M100B2U motors

    1 x PicoPSU 60W connected to the VIA EPIA

    So all up it should control 3 Xbees and 2 unipolar motors, all via USB.

    My questions are regarding powering the robot:

    1. The Phidget Stepper Controller has a separate power input to power the 2 motors. Is it possible to make a connection from one of the PicoPSU's MOLEX connectors to power the motors connected to the PhidgetStepper Controller?

    2. My robot needs to run only for a couple of minutes before recharging. Would any of the following be suitable to connect to the PicoPSU for powering the robot?

    a) http://www.batteryjunction.com/tenergy-11v-4400.html
    b) http://www.batteryjunction.com/tener...nimh-pack.html
    c) http://www.batteryjunction.com/tenergy-31259.html

    Thank you for reading my post, any suggestion are appreciated.
    Matt

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    181

    Re: Powering my robot

    Welcome to the forum!

    The [email protected] is pushing it a bit, but the decently sized LiPo's should do it.

    Just make sure you're using the "Wide Input" power supply and MOST IMPORTANTLY - you need some way to monitor the battery cell voltages. Draining a Li* chemistry battery too far is a Grade-A Bad Idea. (Unless it involves cutting it open and throwing it in salt water...)
    I Void Warranties´┐Ż

  3. Re: Powering my robot

    Thanks a lot Adrenalynn,

    That helps a lot. I have no means of monitoring the battery voltage, so that excludes the Li* batteries. When you say [email protected] is pushing it a bit, do you mean the 9.6, the 4500 or both? Does it just mean the robot won't run that long or does it mean it won't even start up?

    I did a bit of beginner's background reading and I think the 4500 correlates to how long the robot will run. Is this correct?

    So I can use the MOLEX connector to power the motors, as long as I use the wide connector, i.e. the one that usually powers the 5.25" drives?
    Once again thanks,

    Matt

  4. Re: Powering my robot

    Yes, the 9.6 part is the part he means you'll be pushing. The 4500 part is the MAH(milliamp hour) rating which generally indicates how long your robot will run. Eg 4500 about twice as long as a 2250. More specifivally 4500 means you can draw 4.5amps for 1 hour from that batter(after a full charge). Or 2.25amps for 2 hours etc...

  5. Re: Powering my robot

    Thanks Acidtech,
    For taking the time and explaining!

  6. #6
    Join Date
    Sep 2009
    Location
    Madison, WI
    Posts
    40
    Rep Power
    38

    Question Re: Powering my robot

    Quote Originally Posted by Adrenalynn View Post
    The [email protected] is pushing it a bit, but the decently sized LiPo's should do it.

    Just make sure you're using the "Wide Input" power supply and MOST IMPORTANTLY - you need some way to monitor the battery cell voltages. Draining a Li* chemistry battery too far is a Grade-A Bad Idea. (Unless it involves cutting it open and throwing it in salt water...)
    Hi Adrenalynn,

    I'm currently thinking about moving from the NiMH battery packs to LiPo. I know TR has a selection of LiPo batteries and a decent looking charger. However, I know very little about battery tech at this time and so when I read your post I became a little nervous! I wonder if you could explain this a little more, and outside of a LiPo pack and charger (like those that TR sell), what other equipment I might need to purchase?

    I don't mean to hijack this thread if my question appears off-topic here! Please let me know and I'll start a new thread!

    Cheers,
    Stephen

  7. #7
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    102

    Re: Powering my robot

    Hey Stephen,

    I switched over to lipo's on my walkers. It is my understanding that lipos can deliver more power more quickly. I think nicads don't do as well at providing a lot of amps over a short period of time. I wouldn't worry too much about lipos provided you use the appropriate charger and keep the case intact. Outside of that my robot stops working or becomes sluggish when the voltage drops too low.

    Yeah I think they can be scary, and teh charger is a bit intimidating, but you should be fine provided you follow the instructions.

    Also I would love to see a project post about your robot. Seams you are teasing us by asking questions about it. Let the sharing begin.

    Hope this helps.

    DB

  8. #8
    Join Date
    Sep 2009
    Location
    Madison, WI
    Posts
    40
    Rep Power
    38

    Re: Powering my robot

    Quote Originally Posted by darkback2 View Post
    I switched over to lipo's on my walkers. It is my understanding that lipos can deliver more power more quickly. I think nicads don't do as well at providing a lot of amps over a short period of time. I wouldn't worry too much about lipos provided you use the appropriate charger and keep the case intact. Outside of that my robot stops working or becomes sluggish when the voltage drops too low.

    Yeah I think they can be scary, and teh charger is a bit intimidating, but you should be fine provided you follow the instructions.

    Hope this helps.

    DB
    This certainly does help DB. Thanks!

    Quote Originally Posted by darkback2 View Post
    Also I would love to see a project post about your robot. Seams you are teasing us by asking questions about it. Let the sharing begin.
    LOL! I will most certainly begin sharing my project, and soon too! But right now I have a dentist appointment to get to! (No really, I do!)

    Cheers,
    Stephen

  9. #9
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    78

    Re: Powering my robot

    Generally, NiCAD's have a bit lower internal resistance than NiMH. That means that a NiCAD pack will deliver more instantaneous current. The downside is that they have severe memory problems and have to be charged and discharged properly in order to get peak life out of the pack. The "CAD" part of NiCAD stands for cadmium. Cadmium is pretty much outlawed under ROHS so most NiCAD battery packs will be going away.

    NiMH (Nickle Metal Hydride) packs are like the middle of the road between NiCAD and LiPo. They don't have the memory problems that you get with NiCAD but they have a bit higher internal resistance meaning they can't deliver the instantaneous current that a NiCAD can provide. They also don't have the memory problems you get with a NiCAD so you can pretty much charge and discharge them willy-nilly without fear of damaging the pack. Cadmium is not used in NiMH so they don't have the ROHS restrictions you get with NiCAD.

    LiPo is pretty much the "best" of the three batteries listed here. They have a very low internal resistance so they can deliver peak currents easily. They are significantly more efficient so you get much better life per watt used. They are extremely finicky when it comes to charging. If you don't follow the requirements for LiPo charging then there is a very real risk of the battery catching fire. Seriously. Using a well designed charger will minimize the risk to almost nil. They are also pretty particular about discharging. This is what Adrenalynn is alluding to above. If the cell voltage drops below somewhere around 3v per cell then the pack will probably not take a charge again. The damaged pack has a greater risk of catastrophic failure (fire) if you try to charge it. The stuff inside the pack will oxidize really quickly so a damaged pack can catch fire. If you put the pack in salt water for a while it will neutralize the battery so it can be disposed of safely.

    Finally, never, ever, ever charge a battery unattended. Make sure someone is around and the battery is on something fire proof such as a ceramic plate when charging. This goes triple for LiPo's.
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  10. #10
    Join Date
    Sep 2009
    Location
    Madison, WI
    Posts
    40
    Rep Power
    38

    Re: Powering my robot

    jes1510 - Thanks for the explanation regarding LiPo's. So prior to charging a LiPo pack it's probably best, as Adrenalynn mentioned, to check the battery cell voltages. Someone suggested in another thread/post the following item:

    http://www.all-battery.com/valtagewattmeter01019.aspx

    This or something like it is probably worth purchasing for a number of reasons, and checking LiPo's before charging being one of them I guess. (If I find that thread+post again I'll link back to it; I'm pretty sure it was part of a similar discussion.)

    With the voltage and watt meter above, I'm also thinking I'll get the following LiPo battery pack and charger from TR:

    http://www.trossenrobotics.com/store...o-Battery.aspx
    http://www.trossenrobotics.com/store...arter-Kit.aspx

    I'll be able to charge my existing NiMh pack with that charger too... just need to figure out the connectors! (My NiMh has a standard Tamiya on it.)

    Cheers,
    Stephen

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry RC truck robot conversion
    By Orac in forum Project Showcase
    Replies: 24
    Last Post: 11-14-2012, 12:50 AM
  2. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 10:20 AM
  3. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-25-2010, 12:51 AM
  4. Project New Post For Fresh Start On Robot Butler
    By ROBOTMAN in forum Project Showcase
    Replies: 11
    Last Post: 10-31-2009, 01:50 PM
  5. Contest Entry Butler Robot
    By airman00 in forum Project Showcase
    Replies: 11
    Last Post: 07-31-2008, 10:28 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •