Re: Uninterrupted hot swap Lipo battery with other DC source.
Yes, there is a problem with using Diodes. The voltage drop can be a significant problem in some circumstances. In our Brainbot robot, using a Diode pair (with 0.4 volt drop) has a noticable effect on available battery capacity. It also wastes power through heat.
The most annoying problem, though, is you can't use a wall power supply properly. Most 12 volt battery packs have a fully charged voltage somewhat higher than 12.0 volts. I have a 17 amp 12 volt wall power supply that I use to power Brainbot while it is on the bench. When I use that, I have to unplug all the batteries, because the diode pair chooses the source that is a higher voltage rather than the source I "want" it to choose.
My aux. power board (which is now available) solves all of these issues...
- Jon
"The best way to predict the future is to invent it." - Alan Kay, inventor of Smalltalk
Bookmarks