Results 1 to 3 of 3

Thread: Looking for advice on sensor output processing

  1. Looking for advice on sensor output processing

    I've been working with a pressure sensor that has a differential output.

    It has Vin (9v) Gnd, + out and - out. The range of the sensor output appears to be from 0-0.5v when reading from the (+) and (-) outputs.

    Either of these outputs are actually offset by Vin/2 so the output from (-) is 4.5v and the output from (+) varies from 4.5v to 5v.

    I'm looking to shift the output so that it runs from 0 to 0.5v in relation to true ground. I only have 0-9v to play with. In theory I should be able to shift the output signal from + down to Gnd using a simple OpAmp setup - but the only way I've done this in the past is with a differential supply.
    I thought about splitting the supply with a floating ground, but is there an easy way to do it using the same 0-9v supply I'm using for everything else?

    Steve

  2. #2

    Re: Looking for advice on sensor output processing

    I think you're asking how to drop 4.5V. You could use a POT or a resistor.

    What's the name or model of the sensor? What's does your circuit look like... do you have a schematic handy?

    Edit: You might want to look into a AC small signal common emitter amplifier.
    Last edited by MikeG; 02-06-2010 at 07:58 PM.

  3. Re: Looking for advice on sensor output processing

    Thanks for the reply.

    A quick trip to Wikipedia solved it.

    I wanted a single op-amp (LM324 in my case) configured as a differential amplifier.

    That did the trick. Now I get a nice clean 0-5v signal (I scaled it by 10) from the output.

    Steve

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Interesting 10 Important Differences Between Brains and Computers
    By Matt in forum Robot Computers
    Replies: 5
    Last Post: 04-08-2008, 01:44 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •