Results 1 to 8 of 8

Thread: Does this circuit look OK?

  1. Does this circuit look OK?

    I recently tried this touch switch circuit:

    http://www.talkingelectronics.com.au.../touchswtr.gif

    Using a couple of 2n2222 I had lying around. Although I got a response from the first transistor, I could not get the second one to switch and light the LED. I was trying to implement with a 6v supply rather than 9v - does the circuit look OK?

    I have two foil plates that act as the contacts.

    Any advice would be appreciated.

    Steve

    P.S. Can this kind of switch be implemented with just an opamp configured as a comparitor? I would think so, but so far I've not had a lot of luck getting it to work.

  2. #2
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: Does this circuit look OK?

    You're stepping into a frustrating world if you are trying to implement a touch switch like you linked above. That circuit depends on about a billion things lining up correctly to work.

    I would recommend looking at a commercial touch solution if you want something dependable. Here is one by Atmel:
    http://www.atmel.com/products/overview_touch.asp

    Note that I have never used that product but I had a sales rep tell me they are awesome for whatever that is worth. It does look like a neat product.
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  3. #3
    zoomkat Guest

    Re: Does this circuit look OK?

    That is a strange circuit. Just what do you mean by "touch circuit" and what part do the foil plates play?

  4. #4
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: Does this circuit look OK?

    AS it's designed the bas current for the first transistor is supplied by bridging the gap on the contacts which are attached to metal plates. The second transistor conducts once the first starts. If the resistance of your finger is too high then it won't work. It's going to bounce like crazy if it does work. I would avoid that design if possible.
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  5. #5
    Join Date
    Apr 2008
    Location
    Nelson, New Zealand
    Posts
    1,356
    Images
    58
    Rep Power
    74

    Re: Does this circuit look OK?

    Shobley hi: I have used this circuit many times and works very well. its variable voltage is a lot more forgiving.





    This circuit uses a 555 timer as the bases of the touch switch. When the plate is touched the 555 timer is triggered and the output on pin 3 goes high turning on the LED and the buzzer for a certain period of time. The time that the LED and the buzzer is on is based on the values of the capacitor and resistor connected to pin 6 & 7. The 10M resistor on pin 2 causes the the circuit to be very sensitive to the touch.

    your circuit may have a problem in as much that you are reducing the voltage to 6 volts, as that resistor is current limiting to the led that should be changed to about 220ohm for 6v, it may not be turning on due to the 470 ohm.

    The output on this circuit can also go through transistors for a higher out load. you can also omit the buzzer.

    This is another circuit that works and has a higher output load.







    This next circuit uses a schmitt trigger to switch on and off the circuit.
    It turns on an output when the Touch-Plate is touched very briefly and turns off the output when the plate is touched for a slightly longer period of time.




    Hope this helps you out.
    Last edited by 4mem8; 02-14-2010 at 03:24 AM.
    People yearn after this robotic dream, but you can't strip your life of all meaning, emotion and feeling and expect to function.


  6. #6
    zoomkat Guest

    Re: Does this circuit look OK?

    The touch concept here seems very similar to momentary switches actuating relays that make a seal in circuit.

  7. #7

    Re: Does this circuit look OK?

    @shobley
    The circuit is called a darlington pair and it is a very common driver stage. The darlington pair is a simple amp that acts like a single transistor with high input impedance, low output impedance, plus it's cheap and compact. The current gain is pretty high about ~B1*B2. Generally, you see another amplifier stage as the input to a darlington pair and the darlington driving a load. In your case an LED but it's common to see a small motor.

    I'm guessing your circuit is not wired correctly or you do not have enough potential to activate (or saturate) the second transistor's base to emitter junction. The base-emitter-base-emitter has to drop 2(6.5V) for the silicon 2N2222. That is, you have to supply sufficient base current to turn the circuit on. Check your biasing.

    I'm not sure what you're trying to accomplish but the one shot above (4mem8) is a good idea if you want to hold state for some period of time after a switch is closed
    Last edited by MikeG; 02-14-2010 at 06:51 PM. Reason: language/grammar

  8. #8
    Join Date
    Mar 2010
    Location
    Ontario, Canada
    Posts
    105
    Rep Power
    35

    Re: Does this circuit look OK?

    Hi shobley, Can you turn on the LED by shorting the two touch pads?
    CAD Tools: Solidworks 2011. Altium Designer 10
    Micro Controller: ARM7/9, AVR 8bit/16bit, PIC, Nordic nRF, HOLTEK, 51s, NEC
    RF: 2.4G, 433M
    IDE: KEIL MDK3.5, AVR Studio 4, MP LAB, HOLTEK HT-IDE3000, Elipse
    High End: VC, VB, Unix/Linux C/C++, J2ME (For cell phone game), SQL
    Education: EE Master.
    Hobby: RC Helicopter.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Replies: 17
    Last Post: 06-18-2010, 11:49 AM
  2. Question(s) Need help building this circuit on a breadboard
    By FauxReal in forum Robotics General Discussion
    Replies: 5
    Last Post: 02-08-2010, 05:58 PM
  3. A temporary closed switch circuit
    By wireframewolf in forum Off Topic
    Replies: 6
    Last Post: 01-31-2010, 12:13 PM
  4. Parallax Propeller--> Ax-12 circuit help
    By altwolf in forum Humanoids, Walkers & Crawlers
    Replies: 7
    Last Post: 11-15-2009, 01:37 PM
  5. FlexiForce Drive Circuit: Power Supply
    By bioeng in forum Sensors
    Replies: 5
    Last Post: 10-28-2009, 02:28 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •