Results 1 to 7 of 7

Thread: 'J-Dawg One' BRAT-Mech

  1. #1
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    'J-Dawg One' BRAT-Mech

    Named after our infamous 'intern' Jennero! Muahahahaha (He's gonna kill me)

    This BRAT-Mech was ridiculously easy to build, even with a custom pan/tilt setup on it. Currently tweaking some of the code, but I had it built and walking around in about 4 hours or so. Gonna stick with a 2.4ghz PS2 controller and hope for the best, will be a good test of how well it fares in the Robogames environment (since this is an extra one anyway).

    Firing tests work just fine, wifi camera is a crappy airlink one I had extra, but might as well put it to use. Had it walking around for 10+ minutes using a 6v 2300mAh pack without issue, still a decent charge left in the batteries. Once I finish up the code and finish soldering the gun connections, it's 100% operational.

    Basically, it's a weekend project that gets you a combat-ready mech at a low price, not a bad option at all.

  2. #2
    Join Date
    Feb 2009
    Location
    Mesa, AZ
    Posts
    351
    Images
    84
    Rep Power
    50

    Re: 'J-Dawg One' BRAT-Mech

    Shweeet back-up mech! Did you catch the LM thread where I tweaked the BRATMech BBII code to add tilt?
    Last edited by mannyr7; 02-22-2010 at 08:40 PM.

  3. #3
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: 'J-Dawg One' BRAT-Mech

    Quote Originally Posted by mannyr7 View Post
    Shweeet back-up mech! Did you catch the LM thread where I tweaked the BRATMech BBII code to add tilt?
    No, but it sounds like I should check that out, one less thing I need to code :P

    Thanks Manny!

  4. #4
    Join Date
    Apr 2008
    Location
    Nelson, New Zealand
    Posts
    1,356
    Images
    58
    Rep Power
    74

    Re: 'J-Dawg One' BRAT-Mech

    Sweet Mech Andrew. :-)
    People yearn after this robotic dream, but you can't strip your life of all meaning, emotion and feeling and expect to function.


  5. #5
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: 'J-Dawg One' BRAT-Mech

    Which servos are you using?
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  6. #6
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: 'J-Dawg One' BRAT-Mech

    6x 645MG in the legs and 2x 475s for the pan/tilt.

  7. #7
    Join Date
    Jan 2010
    Location
    Texas
    Posts
    58
    Images
    7
    Rep Power
    35

    Re: 'J-Dawg One' BRAT-Mech

    Sweet weekend project. The brat makes for a nice mech. Dont forget us with the action pics!

    Meccano Jay ...
    find me @ http://www.phidgets.com/phorum as well and Happy Building!!



Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Mech Warfare 2010 Draft Rules
    By lnxfergy in forum Mech Warfare
    Replies: 125
    Last Post: 05-24-2010, 12:47 PM
  2. A BRAT based Mech, "Miss Alignment"
    By darrellt in forum Mech Warfare
    Replies: 33
    Last Post: 04-28-2010, 05:39 PM
  3. New Mech: Nostromo
    By webgeek in forum Mech Warfare
    Replies: 109
    Last Post: 04-04-2010, 08:00 AM
  4. BRAT Based Mech?
    By Roboman in forum Mech Warfare
    Replies: 102
    Last Post: 09-18-2009, 06:23 AM
  5. Mech Warfare Rules and Guidelines
    By DresnerRobotics in forum Mech Warfare
    Replies: 238
    Last Post: 07-29-2009, 12:43 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •