Results 1 to 7 of 7

Thread: Hexabot+robot snake

  1. Hexabot+robot snake

    Hi everybody!

    I want to show you 2 unfinished projects (just solidworks models yet....but im working on it)
    both are my first robot projects and is still a loooooooot of work to do, because i didnt started yet the work on the electronics, programming and the manufacturing at all......but the day will come ...
    my hexabot is using 2 ax-12´s and one rx-10 per leg, the robot snake is using 19 hs5055mg´s (2 per segment)
    im not really motivated to explain much of my mechanics now (most of it is anyway intuitive by the pictures), cus im a little bit lazy today.....more of it tomorrow...
    but remember, the mechanical design is unfinished, most of the small sundries up to the "neck" of the hexabot are just not modelled...

    alex

    ps: sorry for my weak english, i come from austria.......

  2. #2
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    138

    Re: Hexabot+robot snake

    Lemme chime in here real quick: What was your reasoning behind using AX-12s *and* RX-10s? The RX-10 technically has less torque, is over double the cost, and complicates your servo communication bus by deviating from the standard half-duplex TTL that the AX-12s use. Would make more sense to use all AX-12s, or step up to RX-28s. I see the RX-10 having very little use (which is why I don't even stock it here at Trossen's store).

  3. Re: Hexabot+robot snake

    well, i know the rx-10 has less torque, BUT its also much faster. (on the other hand, its in germany not double the cost of an ax-12). so i decided to use 2 ax-12 "pushing" the robot away fround the ground, but one servo is just rotating the leg about the z-axis. because it has not to withstand high load, it is not necessary to use a servo with a high torque, but on the other hand it is the most important servo for the speed of the hexabot.........

  4. #4
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    138

    Re: Hexabot+robot snake

    I'd garner that the slight increase in speed doesn't justify the increased cost and complexity of your dynamixel bus (both TTL & RS-485). You'd be surprised at just how fast AX-12s are at 12v, take a look at some of the arbotiX powered quads on this forum for proof.

    Also: The AX-18F will be out shortly, which is faster (97 RPM vs 84 RPM) than the RX-10 for less cost, and on the same TTL network as the AX-12.
    Last edited by DresnerRobotics; 02-26-2010 at 08:10 PM.

  5. #5

    Re: Hexabot+robot snake

    AX-18F? What's this? Is it bracket-compatible with the AX-12+?

  6. #6
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    138

    Re: Hexabot+robot snake

    Identical to the ax-12 formfactor, it's basically an upgraded ax-12 with a coreless motor; faster, slightly more torque. No info on pricing or release date as of yet.

  7. Re: Hexabot+robot snake

    Quote Originally Posted by Tyberius View Post
    Also: The AX-18F will be out shortly, which is faster (97 RPM vs 84 RPM) than the RX-10 for less cost, and on the same TTL network as the AX-12.
    ok, THATS an argument....
    im looking forward to see this servo.....

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry RC truck robot conversion
    By Orac in forum Project Showcase
    Replies: 24
    Last Post: 11-13-2012, 11:50 PM
  2. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 09:20 AM
  3. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  4. Project New Post For Fresh Start On Robot Butler
    By ROBOTMAN in forum Project Showcase
    Replies: 11
    Last Post: 10-31-2009, 12:50 PM
  5. Contest Entry Butler Robot
    By airman00 in forum Project Showcase
    Replies: 11
    Last Post: 07-31-2008, 09:28 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •