Results 1 to 3 of 3

Thread: USB2LTP Converter

  1. Question USB2LTP Converter

    I am making an autonomous robot using the ATMega 16 microcontroller. I have a development board and I have made a programmer (Circuit required to program the microcontroller). Thing is that the circuit that I have made uses a Parallel port. I have a converter which connects the parallel port to the USB port on my laptop (Which does not have a parallel port). However, I cannot seem to find the required drivers that allow me to set the port of the parallel port as LPT(1-3) so I cannot write on the microcontroller. I don't have the time to report it into a USB programmer nor the resources right now.
    Does anyone know where I can get such a driver that will work on Windows XP or Windows 7 such that it gives me LPT1-3 so that I can use a burning software. Or is there any software which will allow me to use the usb2lpt as it is. Right now, on devmgmt.msc, it shows up at "USB Printing Support". I have tried a couple of drivers already but none of them worked.

  2. #2
    zoomkat Guest

    Re: USB2LTP Converter

    I've never seen a USB to parallel port printer adapter that could be bit banged for programming. Your best bet would be to get a parallel port card for the computer or a programmer that operates directly via the serial or USB port.

  3. #3
    Join Date
    Mar 2010
    Location
    Ontario, Canada
    Posts
    105
    Rep Power
    31

    Re: USB2LTP Converter

    Hi aceroom. My experience is: there is no such a thing can do USB to parallel for your application.
    Like zoomkat have said, get a card to do it. for Laptop, get a PCMCIA card to to do it.
    Don't go by "USB to Parallel" on ebay search, it doens't work for you.
    Good luck.
    CAD Tools: Solidworks 2011. Altium Designer 10
    Micro Controller: ARM7/9, AVR 8bit/16bit, PIC, Nordic nRF, HOLTEK, 51s, NEC
    RF: 2.4G, 433M
    IDE: KEIL MDK3.5, AVR Studio 4, MP LAB, HOLTEK HT-IDE3000, Elipse
    High End: VC, VB, Unix/Linux C/C++, J2ME (For cell phone game), SQL
    Education: EE Master.
    Hobby: RC Helicopter.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. programming axon with a-d converter
    By robot maker in forum Software and Programming
    Replies: 21
    Last Post: 07-31-2008, 04:52 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •