Results 1 to 2 of 2

Thread: Multi-function Custom Rf Tilt Transmitter

  1. Multi-function Custom Rf Tilt Transmitter

    Hello Everyone!

    This is a project I have been working on for some time now it is a custom Rf Remote i have built as to control my robots.
    Bill of Materials:
    3.5” Computer Fan
    Radioshack project case
    9v Battery snap
    9v Battery
    4 X AA batteries
    Sumobot PCB
    Board of education
    Basic stamp Sx
    3 X Push-on Push-off switches
    3 X 1/8 in audio port
    Hookup wire
    Spst Toggle switch

    Project Description:
    My robot project is a remote controller and receiver, in the form of a mobile robot, that are interactive. Both have easily accessible IO ports in which to add additional sensors and switches with no rewiring and little code modification. I created this robot because of a personal desire to create a butler robot that can be both entertaining yet useful and expandable.
    The robots motion is controlled using an accelerometer on the transmitter, when you tilt the remote forward the robot moves forward. The robots other features include an integrated mini-fridge, led headlights, and integrated mini-projector. All but the mini-fridge can be activated from the controller. The interactivity of the controller allows the transmitter to also become the receiver allowing the robot to send data to the controller activating led’s, displays, and other periferrals that can be plugged in via the IO ports.
    (Just F.y.i the Robot part of the project has been cancelled due to money issues.)
    I apoloize if the images came out bad, My lowly point and shoot only goes so far.
    Results were inconclusive, the darn thing blew up!

  2. Re: Multi-function Custom Rf Tilt Transmitter

    One more note the transmitter is not finished yet!
    Results were inconclusive, the darn thing blew up!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) AVR Studio help - my first robot
    By grixxlee in forum Robotics General Discussion
    Replies: 6
    Last Post: 02-28-2010, 08:17 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •