Page 3 of 3 FirstFirst 123
Results 21 to 24 of 24

Thread: build my own basic atom pro 28 carrier board

  1. Re: build my own basic atom pro 28 carrier board

    Quote Originally Posted by soldier View Post
    first of all.. sorry for my broken English.. i had build a carrier for BAP28... everything goes fine... i mean the hexapod can be controlled and can walk as usual... but there is one weird problem happening... which is as following detail

    1} buzzer keep beeping(non stop)... actually is continuous sound(same frequency after first beeping)...
    2} the beeping sound is different than the one where the PS2 controller is not connected to the Atom properly
    3} the sound also got a little bit different from the one when we apply power
    4} during the continuous beeping sound.. when i press other button such as start button... it will still appear original start button's beeping sound pattern as usual (mix with the continuous beeping)
    5} but the buzzer goes normal(pin9 LOW) and fine after i reset it or press square button(ps2) for the (1st press and 2nd press after start button)
    6} every time apply power... it will keep beeping(pin9 HIGH) until i press reset or square button (1st press and 2nd press after start button)
    7} but the beeping comes again(pin9 HIGH) if i press square button(3rd press and 4th press)... and will goes normal(pin9 LOW at 5th press and 6th press)...
    8} the reset button can be press at anytime and works fine(pin9 LOW) anytime i press it
    9} conclusion is for square button (1st and 2nd press- Pin9 LOW... 3rd and 4th press- Pin9 HIGH... 5th and 6th press- Pin9 LOW and so on)

    but the hexapod can be controlled as usual... please help...

    what happen actually??? why i need to press reset or square button(1st,2nd,5th,6thpress)??? please help.. thanks
    i had edit my post cos got some changes...
    im using the code form link (http://www.lynxmotion.com/images/html/build159.htm)
    for the code.. if im not mistaken.. it will LOW on pin9 if i press nothing right?? and will HIGH only for few second if certain button is pressed... but why mine keep HIGH on pin 9 while im using the same coding?? and work properly if i attach to the BAP28 to the bot-board II

  2. Re: build my own basic atom pro 28 carrier board

    finally problem solved... its hardware problem...
    thanks for u all guys
    i should cal u all guru... haha
    thanks again
    Last edited by soldier; 03-20-2010 at 10:19 AM.

  3. #23
    Join Date
    Jul 2008
    Location
    Chicago
    Posts
    307
    Rep Power
    55

    Re: build my own basic atom pro 28 carrier board

    What was the problem?

    Ill take a guess here but maybe the buzzer was made to be constantly on?

  4. Re: build my own basic atom pro 28 carrier board

    my buzzer will keep beeping once voltage is supplied to it....
    suppose i should just use transducer which needs PWM supplied to it to make it go beeping... so now i already change my buzzer to transducer... and it works fine now... that's the problem... thanks

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Basic Atom proM and Atom Pro
    By 4mem8 in forum Robot Computers
    Replies: 6
    Last Post: 02-12-2010, 03:53 PM
  2. News/Announcement BASIC Atom Pro28 for sale!!
    By innerbreed in forum Garage Sale
    Replies: 0
    Last Post: 07-31-2009, 03:59 PM
  3. Question(s) Basic Atom Pro / PulsinRead issues / How to invert some inputs.
    By LikWidChz in forum Software and Programming
    Replies: 3
    Last Post: 03-31-2009, 05:35 PM
  4. Basic atom problem
    By sam in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 12-26-2008, 07:08 PM
  5. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •