Results 1 to 2 of 2

Thread: RX-28 and RX-64 Open-Source (Python) Libraries Available

  1. RX-28 and RX-64 Open-Source (Python) Libraries Available

    Having read extensively through the forums, I suppose I'll share...

    I recently invested a decent amount of time overhauling my lab's open-source software for controlling Robotis RX-28 and RX-64 servos from a PC. The code is written entirely in Python and is thread-safe, so that multiple servo objects can be controlled / queried "simultaneously" on the same USB2Dynamixel bus (within the same process). The library should function on Linux, Mac, and Windows (yay, python!), and the only dependency is PySerial for communications. ROS (Robot Operating System) support has also been created.

    You can find the library and details, here [Hizook.com]

  2. #2
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: RX-28 and RX-64 Open-Source (Python) Libraries Available

    Very sweet! I don't have any of those servos but +rep for sharing. Nice work!
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •