Results 1 to 5 of 5

Thread: New Mac User, with CNC Dreams...

  1. New Mac User, with CNC Dreams...

    Hello... Just found this Company & Group Forum.... I am attempting to build a CNC...problem is I'm on a MAC and there is no software for mac that will run a CNC. I have been reading about the 1062 controller, and it may be the answer to my problem. Although I am not a programmer... I am a designer.... i noticed that the controller can take instruction from Flash using Action Script. In my imaginings... i have visions of creating ( or importing ) my design projects in Flash.... then being able to output them through the usb port to the 1062 controller... and having a fantastic new CNC..... can someone tell me....am I being too hopeful...or even delusional?...lol At any rate... and direction that anyone can give me would be much appreciated. ie... programmers?..websites?..tutorials? Programs??? ( Naww... programs is asking wayyy too much me thinks...lol )

    Thanks in advance

    Imacman

    Newfoundland, canada

  2. #2
    Join Date
    Jul 2008
    Location
    Chicago
    Posts
    307
    Rep Power
    44

    Re: New Mac User, with CNC Dreams...

    CNCZone.com is your best bet for all the knowledge you need to build your own CNC. They have a great forum about all types of CNC equipment.

  3. #3

    Re: New Mac User, with CNC Dreams...

    If you have an Intel Mac (one of the newer models) you can install Windows along with Mac OS via Bootcamp. Thats what I use for Roborealm, Visual Studio etc.

  4. Re: New Mac User, with CNC Dreams...

    Yes I was thinking windows on my MAC would be an option, but there's no Serial port on an Imac.. I do have a few G3's, G4's & G5 PPC's here...but they won't take windows...lolol.......

    I was hoping to use the controller as the controller for a CNC woodworking machine... but I'm be told by the CNC people that the specs on the Controller are insufficient.... and that it can only control one axis at a time... Plus there is some sort of latency issue with USB Ports.... So I'm still searching...... I am in contact with a company Simlab Soft... that makes a great piece of 3D design software called Simlab Composer for MAC..... if they could just get this software to convert the 3D design to G-Code some how... then output it say over the Ethernet port on the MAC..... then the world would be a better place!.... theres a huge market for such a set up. I'm that desperate right now... that I'm even looking to see if I can somehow control the three stepper motors using MIDI signals..... they operate with no latency on a Mac.!...lol I've even just signed up for the RepRap project, I may build one to educate myself to it all. Any advice anyone???

    Imac

  5. Re: New Mac User, with CNC Dreams...

    I use an old Dell 1 GHz P3 laptop running Windows XP as the controller on my CNC Sherline milling machine. You can probably pick up a laptop with those specs for a couple hundred dollars, and less if you used an old desktop.

    - Jon
    "The best way to predict the future is to invent it." - Alan Kay, inventor of Smalltalk

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 09:20 AM
  2. Cnc cad program and hardware opinions requested
    By science_geek in forum Software and Programming
    Replies: 4
    Last Post: 06-14-2009, 11:39 AM
  3. Which CNC system to save for?
    By Sienna in forum Mechanics / Construction
    Replies: 13
    Last Post: 06-24-2008, 07:33 AM
  4. CNC mill for robot parts
    By asbrandsson in forum Mechanics / Construction
    Replies: 33
    Last Post: 03-29-2008, 09:31 PM
  5. Apple's Designer Scared!
    By srobot in forum Off Topic
    Replies: 8
    Last Post: 03-14-2008, 12:08 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •