Results 1 to 4 of 4

Thread: Powering a Roboard

  1. Powering a Roboard

    Hi,
    Would it be possible to power this RoBoard: http://www.roboard.com/RB-110.htm
    with this battery pack: http://airsoft-club.com/shop/batteri...battery-gp850c
    ?

    I'm not concerned with whether or not the plug fits and I only need to power the board for 15mins.

    The RoBoard requires:
    Power Consumption +5V @ 400mA
    Power Input DC-in 6V to 24V

    and the battery pack has these values:
    11.1V 1200mAh 20C

    Would that do the trick?
    Thanks for your help!

  2. #2
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Re: Powering a Roboard

    Yes that should power it fine. Keep in mind that it wouldn't work for Hobby servos however, which have a 6v requirement.

  3. #3
    Join Date
    Feb 2009
    Location
    Mesa, AZ
    Posts
    351
    Images
    84
    Rep Power
    54

    Re: Powering a Roboard

    Does the Roboard have provisions to run servos off their own separate power supply?

  4. Re: Powering a Roboard

    Thanks Tyberius,
    For the good news and the hint with the servos.
    I was actually planning to purchase this (http://www.trossenrobotics.com/p/phi...ontroller.aspx), connect it to the same power supply and hook it up to the RoBoard via USB.
    If I understood the Phidget manual correctly, then the controller should take care of adjusting the voltage for the stepper motor. Hopefully this works.

    @mannyr7: I'm not sure but here is what it says in the specs:
    Note: Servos are powered directly from the input voltage, so a 6v power supply is needed for most hobby servos to function safely.
    I hope this answers your question.

    Cheers,
    Matt

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Can Roboard capture (read) PWM from an RC receiver (RC Servo lib)?
    By John Elliott in forum Robot Computers
    Replies: 19
    Last Post: 01-10-2010, 08:50 AM
  2. Roboard Question
    By marsman in forum Robot Computers
    Replies: 1
    Last Post: 10-22-2009, 11:43 AM
  3. Roboard questions
    By mx270a in forum Robot Computers
    Replies: 13
    Last Post: 07-23-2009, 11:43 AM
  4. Roboard Questions
    By sniperscope in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 05-07-2009, 12:19 PM
  5. Discussion My Roboard: First Thoughts
    By WGhost9 in forum Robot Computers
    Replies: 14
    Last Post: 04-15-2009, 07:45 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •