Results 1 to 5 of 5

Thread: Motion sequencing in RoboPlus Motion?

  1. Motion sequencing in RoboPlus Motion?

    Some motions from examples I have downloaded to roboplus for my comprehensive kit CM-5 automaticaly sequence. For example, I click play on motion 5, and the robot automatically cycles throught motions 5, 6, 7, 8, and 9. This is used for routines that require more than the 7 steps availible per motion.

    Does anyone here know how I can sequence motions like that in the motion editor of RoboPlus?

  2. #2
    Join Date
    Aug 2008
    Location
    Iowa City, IA
    Posts
    390
    Rep Power
    44

    Re: Motion sequencing in RoboPlus Motion?

    I don't have it installed on this machine so I can check, but.. don't you just need to set the "NEXT" and "END" fields of a motion?

  3. Re: Motion sequencing in RoboPlus Motion?

    I do not know, I have never done it. How do I set the NEXT and END fields? Where are they?

  4. #4
    Join Date
    Mar 2008
    Location
    Knoxville, TN
    Posts
    274
    Images
    35
    Rep Power
    52

    Re: Motion sequencing in RoboPlus Motion?

    the NEXT and END fields are used to tell a page what to do after it's done, or what to do when it's told to stop playing.

    Example:

    Page1, Next: 2, End 2
    Page2, Next: 3, End 3
    Page3, Next: 4, End 4
    Page4, Next: 5, End 5
    Page5, Next: 2, End 6
    Page6, Next: 0, End 0

    So, you start at page 1, it goes into a loop and loops pages 2-5, if it's told to stop playing, it'll finish the loop, then jump to page 6 which is a finial sequence (normally your default standing pose)

    Thanks, Connor

  5. Thumbs up Re: Motion sequencing in RoboPlus Motion?

    Thank you! I have been trying to figure this out for a long while.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Trouble with CM-5 firmware for RoboPlus
    By milw in forum Software and Programming
    Replies: 3
    Last Post: 01-25-2010, 10:14 PM
  2. Bioloid Roboplus beta software from Robotis!
    By altwolf in forum Humanoids, Walkers & Crawlers
    Replies: 15
    Last Post: 09-17-2009, 10:31 AM
  3. Motion play back in Bioloid
    By brijesh in forum Mech Warfare
    Replies: 0
    Last Post: 11-25-2008, 02:43 PM
  4. A doubt on how Robotis company creates the motion files?
    By kbv2842 in forum Humanoids, Walkers & Crawlers
    Replies: 9
    Last Post: 04-28-2008, 09:52 AM
  5. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •