Results 1 to 8 of 8

Thread: Spring Cleaning: Tri-Track, Arduino, Sensors

  1. #1
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    134

    Spring Cleaning: Tri-Track, Arduino, Sensors

    I've got a bunch of stuff that's just sitting around here doing me no good, priced to sell, hopefully others can put this stuff to use. I can only accept payment through paypal. All items will be shipped USPS (Continental US addresses only!). PM me if you are interested, first come, first served.

    NOTE: ALL ITEMS IN GOOD WORKING CONDITION, HOWEVER DUE TO THE NATURE OF THE HOBBY, I CANNOT ACCEPT RETURNS, SINCE I CANNOT BE ASSURED YOU DIDN'T BLOW SOMETHING UP.

    -Fergs

    First up: I have 2 Pololu 3pi robots for sale, each comes with a black expansion deck (with LCD cutouts). These are nearly brand new, both in box, one still in wrapper inside the box, expansion decks are still in original plastic wrapping. Would be $110 new. Each is $70, shipped.

    Next: A lynxmotion Tri-Track. Fully Assembled, never used (project it was intended for got canceled). $190 shipped. I will probably unbolt the center plates so that it fits easier into a box for shipment. Also includes small bag of hardware for attaching control boards.



    Next Up: A solarbotics motors/tracks on Robotshop frame -- NO ELECTRONICS. Sells for $84 new, $60 shipped assembled and with motors already wired to go! The electronics shown are NOT INCLUDED. This little guy is in almost brand new condition.




    Next: Set of 3 SRF-02 I2C sonar ranging sensors. Nearly new, with wires attached. $50 shipped.



    Next up: Eltec Pyroelectric sensor, great for fire fighting robots or tracking people. This is not like your average Pyroelectric, it has a very high update rate. Brand new, sells for $95 from Acroname, $60 shipped.


    Last, prototype frames from SMALdog. I've open sourced SMALdog's IK and motion engine (and NUKE will soon support custom 3DOF Mammal IK). I've got 4 extra frames, these are identical to SMALdog's. I don't particularly want to hang onto them, nor do I want to throw them out. May have extra holes in teh center of the platform, markings, etc. May show small stress cracks on bends, but are all plenty strong enough for building your own SMALdog. Probably also need to be cleaned up for sharp edges. $1 + $5 shipping = $6 shipped.

    Last edited by lnxfergy; 07-23-2010 at 07:53 PM.

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    134

    Re: Spring Cleaning: Tri-Track, Arduino, Sensors

    Prices reduced above. Also note, I can combine shipping on multiple items, so knock $5 off each subsequent item after the first.

    -Fergs
    Last edited by lnxfergy; 07-23-2010 at 07:53 PM.

  3. #3
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    134

    Re: Spring Cleaning: Tri-Track, Arduino, Sensors

    SSC-32 and AVRISP2 are sold.

    -Fergs

  4. #4
    Join Date
    Apr 2008
    Location
    Jacksonville, FL
    Posts
    144
    Rep Power
    48

    Re: Spring Cleaning: Tri-Track, Arduino, Sensors

    Thanks Fergs!! I can't wait to put them to good use.

    Jax
    If a robot has a screw it must be removed and then mods must be made to it.
    Jax

  5. #5
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    134

    Re: Spring Cleaning: Tri-Track, Arduino, Sensors

    Pololu Motors are gone.

    -Fergs

  6. Re: Spring Cleaning: Tri-Track, Arduino, Sensors

    A lynxmotion Tri-Track. still available?
    World of Warcraft
    www.ofhellfire.com
    MC Raiders!! We ant got no life!!

    Da Newb, and yes this is my bear butt.....

  7. #7
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    134

    Re: Spring Cleaning: Tri-Track, Arduino, Sensors

    Quote Originally Posted by Hellfire View Post
    A lynxmotion Tri-Track. still available?
    Yes it is.

    -Fergs

  8. #8
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    134

    Re: Spring Cleaning: Tri-Track, Arduino, Sensors

    Prices lowered on several of the remaining items above.

    -Fergs

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  2. Looking to buy lynxmotion tri track chassis
    By Spartan001 in forum Garage Sale
    Replies: 5
    Last Post: 10-12-2009, 11:11 PM
  3. tri track mod
    By farmBot in forum Robotics General Discussion
    Replies: 6
    Last Post: 11-08-2008, 02:38 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •