Results 1 to 3 of 3

Thread: How should I write an "AX-S1-like" program for querying CM-510 sensors?

  1. #1

    Question How should I write an "AX-S1-like" program for querying CM-510 sensors?

    I'm trying to read the new Bioloid Premium sensors from USB2dynamixel (or serial port with Toss mode). There are several ways...

    But I think that the most interesting way would be writing a C program by which the CM-510 acts as another "dynamixel" device, answering the queries directed to him (ID 200, 0xC8). That is, using it like the "old" AX-S1 to get the sensors values.

    It should be possible because there is a "monitor" command in the CM-510 firmware that show all packets sent/received from the usb2dynamixel. I have tried it but it doesn´t work .
    Last edited by siempre.aprendiendo; 05-23-2010 at 04:59 PM.

  2. #2

    Re: How should I write an "AX-S1-like" program for querying CM-510 sensors?

    It works!

    Well, at least I have managed to create a toss mode program, and then it has been very simple to create a "device mode" for CM-510.

    Now I will clean up the code and write the "answers" with the sensors values

    Finally I have used the new Robotis libraries.
    Last edited by siempre.aprendiendo; 05-23-2010 at 05:12 PM.

  3. #3
    Join Date
    Apr 2009
    Location
    Cohoes, NY
    Posts
    209
    Images
    21
    Rep Power
    40

    Post Re: How should I write an "AX-S1-like" program for querying CM-510 sensors?

    Quote Originally Posted by siempre.aprendiendo View Post
    I'm trying to read the new Bioloid Premium sensors from USB2dynamixel (or serial port with Toss mode). There are several ways...

    But I think that the most interesting way would be writing a C program by which the CM-510 acts as another "dynamixel" device, answering the queries directed to him (ID 200, 0xC8). That is, using it like the "old" AX-S1 to get the sensors values.

    It should be possible because there is a "monitor" command in the CM-510 firmware that show all packets sent/received from the usb2dynamixel. I have tried it but it doesn´t work .
    I believe that CM-510 has a build-in AX-S1. The main difference being able to change sensors.

    My $.02.

    SA

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •