Results 1 to 4 of 4

Thread: Second Rover Build

Hybrid View

Previous Post Previous Post   Next Post Next Post
  1. Second Rover Build

    This is my second rover build. I used another Traxxas chassis for this only I used a rock crawler truck, the Summit. It not only is lower geared but has a two speed transmission and locking differentials. The Slash chassis that I used last time did not work real well as we burned up the motor during testing due to the weight and speed of the rover. I used the same video system with a bit better battery.

    For the video system I used to IP cameras, a Panasonic BB-HCM531A and a Panasonic BL-C1A. The BB-HCM531A is a P/T for the front drive and surveillance camera and the BL0-C1A is a fixed rear mounted reverse camera. This is connected to a Linksys WRT54GL router flashed with DD-WRT which in turn have two high gain antennas.

    The body is built from polycarbonate for less weight and more impact resistance. Because it is polycarbonate, I could attach the electronics directly to the body, again saving weight.

    I now have about $2500 in the build with the more expensive Summit chassis. We are getting about an hour run time on the batteries we currently have. An upgrade to LiPO batteries will help that and weight issues. We are getting about 1100 feet line-of-site control and about 250 feet through two walls inside a building. My next project is to convert the servo and speed controller of to a computer via a serial port added to the WRT54 router, hence my other post.

    Tristan
    Last edited by Sundsted; 07-07-2010 at 02:35 PM. Reason: Adding photos

  2. #2
    Join Date
    May 2010
    Location
    Fairbanks, AK
    Posts
    16
    Rep Power
    33

    Re: Second Rover Build

    Very nice. This one should be more stable and easier to control than the slash version. You're also getting descent range and excellent runtime. Good job.

  3. #3
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    75

    Re: Second Rover Build

    Nice work! I'm digging that custom body. Can you elaborate a bit on your setup? I see what looks like a router (I'm guessing flashed with DDWRT?) but I can't really tell what else you have going on in there.
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  4. #4
    Join Date
    May 2010
    Location
    Fairbanks, AK
    Posts
    16
    Rep Power
    33

    Re: Second Rover Build

    Looks like he migrated most of the gear from his other rover.
    http://forums.trossenrobotics.com/showthread.php?t=4099

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-25-2010, 12:51 AM
  2. Project starting a new rover project
    By csdude in forum Rovers
    Replies: 22
    Last Post: 01-10-2010, 01:10 AM
  3. Fit-Bot - a Fit-PC based rover
    By coppertubing in forum Robot Computers
    Replies: 9
    Last Post: 10-06-2009, 09:32 AM
  4. Question(s) Rover Money $$$$ ?
    By Moonbase.inc in forum Projects For Request and/or Sale
    Replies: 12
    Last Post: 01-19-2009, 02:33 AM
  5. Project Need Advice: Laptop based autonomous rover
    By Merik in forum Robotics General Discussion
    Replies: 2
    Last Post: 01-11-2009, 04:53 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •