Results 1 to 5 of 5

Thread: Electronic Brick to axon!

  1. Exclamation Electronic Brick to axon!

    is it possable to conect the Electronic Brick Chassis (V1.1) to the axon via UART cables? i am very inexperienced,i am making my first robot. do you need extra coding or something like a connection frequency?this is quite ugent to weather i shoud buy an electric starter kit and what i shoud buy with it

  2. #2

    Re: Electronic Brick to axon!

    I'm sure someone will correct me but it looks like the Electronic Brick Chassis (v1.1) is designed from an ardunio? The brick exposes the Ardunio's pins through 10 and 3 pin connectors. The Brick does not have any smarts, it's just a pass-through. I guess it would work for an axon if the header pins are similar.

  3. #3
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    149

    Re: Electronic Brick to axon!

    Quote Originally Posted by MikeG View Post
    I'm sure someone will correct me but it looks like the Electronic Brick Chassis (v1.1) is designed from an ardunio? The brick exposes the Ardunio's pins through 10 and 3 pin connectors. The Brick does not have any smarts, it's just a pass-through. I guess it would work for an axon if the header pins are similar.
    You're correct. Though the Axon has breakouts for I/O that provide 3 pin connections, which is all the Electronic Brick Chassis does anyway. Trying to use it would be largely redundant.

  4. Re: Electronic Brick to axon!

    well,are there eny other lcds that are UART compatable? cuz i just fownd that was the only part i cant find in non electronic brick format.i know it exsists tho

  5. #5
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    149

    Re: Electronic Brick to axon!


Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Axon Based Hexapod Control (with a SSC-32 helper)
    By WGhost9 in forum Project Showcase
    Replies: 1
    Last Post: 01-14-2010, 12:46 AM
  2. Problems connecting PS2 controller to Axon
    By JadeKnight in forum Arbotix, Microcontrollers, Arduino
    Replies: 11
    Last Post: 09-26-2009, 07:21 PM
  3. Question(s) Axon Programming Questions
    By WGhost9 in forum Robot Computers
    Replies: 20
    Last Post: 07-06-2009, 05:15 PM
  4. Question(s) Axon to SSC 32
    By WGhost9 in forum Robot Computers
    Replies: 8
    Last Post: 06-25-2009, 08:52 PM
  5. How can I fry my Axon?
    By Resilient in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 02-19-2009, 05:09 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •