Results 1 to 10 of 10

Thread: Connecting 5mm Motor Shaft To

  1. Connecting 5mm Motor Shaft To

    I'm trying to connect a 5mm motor shaft on a unipolar stepper to .125" square drive shaft.

    I was hoping to find some type of mounting hub that would allow me to do this -- anyone seen anything like that?

    It's okay to tell me I've just started off on the wrong foot and just get a motor with a square shaft.

  2. #2
    Benjamin Guest

    Re: Connecting 5mm Motor Shaft To


  3. Re: Connecting 5mm Motor Shaft To

    Thanks! I appreciate the suggestion.

  4. #4

    Re: Connecting 5mm Motor Shaft To

    If the motor shaft is square I see no reason why a standard clamp on type flex
    coupler wouldn't work. just measure from corner to corner and get at coupler with
    that ID size.

    not sure I would use it for high torque applications, but should be fine for stepping motors.

    Tommy
    Last edited by Tommy_T; 09-26-2010 at 06:02 AM.

  5. #5
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    97

    Re: Connecting 5mm Motor Shaft To

    You could always cut a hub using a lathe. If you don't have one check your local community college or skill center. They sometimes like to have jobs for students to do. For the square shaft make 4 set screws. That way you can clamp down on it pretty evenly. If the square shaft is big enough you can drill 4 divots into it so that the set screws have something to sink into.

  6. #6
    zoomkat Guest

    Re: Connecting 5mm Motor Shaft To

    If the load isn't too high, you might be able to make a little shaft coupling using heat shrink tubing. After it is made, a little super glue might be needed on the round shaft.

  7. #7

    Re: Connecting 5mm Motor Shaft To

    For making square holes you need a square broach.

    Their expensive.

    http://www.mcmaster.com/#square-broaches/=90zqy8

  8. #8
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    97

    Re: Connecting 5mm Motor Shaft To

    Thats why I suggested the four set screws. Drill the hole bigger then the square shaft and then clamp down on it with the 4 set screws...saves a bit of money. You could also cut the shaft in half and mill out a channel in each side and then clamp the two halves together.

  9. Re: Connecting 5mm Motor Shaft To Square Drive Shaft

    Everyone, thanks for the helpful suggestions! What I discovered was that the basis for my question was wrong -- I started out combining some components from Phidgets and the unipolar stepper motor available on trossen with some components from VEX -- the vex components / gears all fit the square drive shafts.

    Anyway, I ended up just getting gears from McMaster-Carr for my round motor shafts and connecting it to the drive shaft gear to gear.

    The heat shrink tubing idea is great -- I'm definitely gonna tuck that one away.

    Thanks for the help!

  10. #10
    zoomkat Guest

    Re: Connecting 5mm Motor Shaft To

    The heat shrink tubing idea is great -- I'm definitely gonna tuck that one away.
    When I was a kid, the kits with small motors used a small piece of rubber tubing that was pressed on to the motor shaft and the connected shaft to couple them together. Small vinal tubing used for aquariums might work, or something similar molded from silicone sealant to make a press on coupling.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. [Need help with connecting Phoenix!]
    By MSK Mech Commander in forum Humanoids, Walkers & Crawlers
    Replies: 10
    Last Post: 10-15-2009, 01:53 AM
  2. Question(s) Hexapod SSC-32 connecting to Lynxterminal
    By explojr in forum Arbotix, Microcontrollers, Arduino
    Replies: 33
    Last Post: 10-11-2009, 01:43 AM
  3. Problems connecting PS2 controller to Axon
    By JadeKnight in forum Arbotix, Microcontrollers, Arduino
    Replies: 11
    Last Post: 09-26-2009, 07:21 PM
  4. Question(s) Connecting to PC
    By Remus in forum Software and Programming
    Replies: 12
    Last Post: 06-19-2009, 11:12 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •