Results 1 to 3 of 3

Thread: Trying PyPose with a USB2Dynamixel

  1. #1
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    49

    Trying PyPose with a USB2Dynamixel

    Hello Fergs,

    I'm finally getting around to trying out your ArbotiX software but at the moment all I have is a USB2Dynamixel. I am starting with the PyPose editor and I set the baud rate to 1000000 instead of 38400. I have 11 servos on my bus and when I do a "capture", the sliders move to the appropriate positions in the PyPose editor window and I get the "captured pose!" status message. So far so good. However, if I move the servos manually to a new position, highlight my captured pose, then click the "set" button to see if the servos will move to the pose, the servos do not move and I get the following console messages:

    Setting pose...
    Setting pose size at 11
    Fail Read
    Fail Read
    Fail Read
    Fail Read

    Any thoughts on what might be going on? Should it even work with a USB2Dynamixel or only with the ArbotiX?

    Thanks!
    patrick
    The Pi Robot Project
    http://www.pirobot.org

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    127

    Re: Trying PyPose with a USB2Dynamixel

    In addition to setting the baud to 1mbps, you need to set "interpolation" to false, as the USB2Dynamixel cannot do onboard smooth interpolation.

    Eventually, we'll have an entirely new port dialog with these options available there, in the meantime, you'll have to edit the code.

    -Fergs

  3. #3
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    49

    Re: Trying PyPose with a USB2Dynamixel

    That was it exactly--thanks!

    --patrick
    The Pi Robot Project
    http://www.pirobot.org

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Arbotix & PyPose
    By Suicidal.Banana in forum Software and Programming
    Replies: 90
    Last Post: 12-21-2017, 04:12 PM
  2. Strage Problems with usb2dynamixel
    By isermann in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 03-21-2010, 05:29 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •