Page 29 of 29 FirstFirst ... 4192526272829
Results 281 to 288 of 288

Thread: More Mule then Rover?

  1. #281

    Re: More Mule then Rover?

    with all the snow and Ice we've had so far this year I had to put
    something together for more power. 6hp engine runs the alternator good, just very noisy.

    Click image for larger version. 

Name:	IMG_1085.jpg 
Views:	397 
Size:	119.6 KB 
ID:	7673
    Last edited by Tommy_T; 02-21-2021 at 05:42 AM.

  2. #282

    Re: More Mule then Rover?

    That looks like a monster :-)
    What poor lawn tractor had to donate its heart like that?

  3. #283

    Re: More Mule then Rover?

    jwatte, even better 6hp for $20 on facebook marketplace, came from pressure washer with bad pump.

    only has pull start so can't see it surviving the winter.

    Click image for larger version. 

Name:	cutting1.jpg 
Views:	314 
Size:	24.5 KB 
ID:	7678
    Last edited by Tommy_T; 03-04-2021 at 07:14 PM.

  4. #284

    Re: More Mule then Rover?

    Sounds like a good deal!

  5. #285

    Re: More Mule then Rover?

    Click image for larger version. 

Name:	tempsnip.png 
Views:	412 
Size:	296.0 KB 
ID:	7674it was cheap, but I hate that it's needed.(so noisy)
    Last edited by Tommy_T; 03-01-2021 at 09:26 PM.

  6. #286
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: More Mule then Rover?

    Is that an attempt to add electric start to the little 160~200cc Honda GCV? Or did you lose yet another wheel due to shaft shearing apart?

    I'm kinda wondering what would be necessary to better silence the exhaust of a GCV engine. I still have not built an electric alternative to my >12 year old Honda/Craftsman lawnmower, and it has always been annoyingly loud even with earplugs.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  7. #287

    Re: More Mule then Rover?

    Is that an attempt to add electric start to the little 160~200cc Honda GCV? Or did you lose yet another wheel due to shaft shearing apart?
    tician, no that image was put there by mistake.

    a few years ago I went to 1" shafts, and 1" ID hubs, I have not had any 1" shaft failures yet.(sweet)

    I'm kinda wondering what would be necessary to better silence the exhaust of a GCV engine.
    I've tried a few things(enclose the engine, add mufflers and used high temp insolation) but, was still
    too noisy for me. I hope to have a fix by next winter.

    last spring a made a e-bike, then I made a few 24v lipo battery packs, I may look at lipo packs for the mule.

    the kickstand was electric(linear actuator)
    and backup camera display on the handlebars
    motor on both wheels, front motor geared for hill climbing, back motor geared to street(25mph).
    used freewheel sprockets on both so could switch back and forth on the fly.
    very fun to ride and could even do some work.

    Click image for larger version. 

Name:	bike2.PNG 
Views:	319 
Size:	974.2 KB 
ID:	7677

    Click image for larger version. 

Name:	bike.PNG 
Views:	322 
Size:	1.50 MB 
ID:	7675

    Click image for larger version. 

Name:	IMG_0262.jpg 
Views:	323 
Size:	122.1 KB 
ID:	7676
    Last edited by Tommy_T; 03-03-2021 at 08:51 PM.

  8. #288

    Re: More Mule then Rover?

    the bucket worked sweet last few winters so I'm not making any big changes.



    first small change- to help put more weight on the bucket for getting ice off the road
    I added dead weight to the front of the mule, this winter I'm replacing the dead weight
    with a few batteries.
    Click image for larger version. 

Name:	IMG_2050.jpg 
Views:	2 
Size:	108.8 KB 
ID:	7690Click image for larger version. 

Name:	IMG_2052.jpg 
Views:	3 
Size:	116.2 KB 
ID:	7691Click image for larger version. 

Name:	IMG_2054.jpg 
Views:	3 
Size:	102.2 KB 
ID:	7692


    I also found a new 8hp briggs engine with a .5amp alternator and electric start.
    Click image for larger version. 

Name:	IMG_2056.jpg 
Views:	2 
Size:	114.6 KB 
ID:	7693

Thread Information

Users Browsing this Thread

There are currently 6 users browsing this thread. (0 members and 6 guests)

Similar Threads

  1. Project Second Rover Build
    By Sundsted in forum Rovers
    Replies: 3
    Last Post: 07-17-2010, 04:04 PM
  2. First rover bot project!
    By Carlcox89 in forum Rovers
    Replies: 4
    Last Post: 07-01-2010, 06:55 PM
  3. Fit-Bot - a Fit-PC based rover
    By coppertubing in forum Robot Computers
    Replies: 9
    Last Post: 10-06-2009, 09:32 AM
  4. Xan's Rover with Arm
    By Xan in forum Rovers
    Replies: 14
    Last Post: 07-18-2009, 02:16 AM
  5. Discussion Rover Kits
    By LinuxGuy in forum Rovers
    Replies: 0
    Last Post: 04-02-2008, 05:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •