Results 1 to 3 of 3

Thread: Creeper needs attack mode

  1. #1
    Join Date
    Apr 2016
    Location
    Detroit Region
    Posts
    13
    Rep Power
    21

    Creeper needs attack mode

    Hey fellow Trossenites,

    I built a Minecraft Creeper prop (see my profile) for Halloween a couple of years ago with the intention of fully robotizing it, am I'm planning for this year now.

    I'm looking for recommendations on a mobile platform that can move Curt (the Creeper) around and scare small children when they get too close on Halloween night. Or any other night. Or day. I managed to get Curt moving with 2 cheap-o plastic tracked chassis controlled with a sketch running on an Arduino mega; I got him to turn his head back and forth and travel in a square on my hardwood floor. it also has a dozen or so high powered LEDs inside for exploding and such and a pretty loud speaker also for exploding and what ever Curt might try to say.

    I see there are a lot of awesome robots, and I found ROS, and I think I want to learn it, I got pretty deep into Arduino and think I can make the leap (I'm not a professional programmer).

    I don't have a huge budget, but I'm looking for the most high level system I can get because what I want to do is make use of it for fun, not do serious research with it.

    At a minimum, I want Curt to wander around my flat concrete driveway at idle, and maybe out onto the sidewalk and back. This sounds to me like it needs SLAM. When encountering fellow Minecraftians I'd like Curt to interact with them in various ways. Such as exploding. or Not, maybe if they hit him with a sword or arrow. I think I will be comfortable with programming some interactivity but ROS and the navigation will be all new. I'd also like to be able to control Curt by remote at any time.

    At a 2nd level, I'd like Curt to chase people wherever they go, across the yard and onto the road and wherever they may go, hide behind objects, just like in the game.

    I estimate Curt weighs around 25lb with 12V Lipo battery. A lot of the chassis I've seen handle a lot more than that, and are also beyond my current budget. I'd like to keep it around $1000 for now. The base of Curt is 24"x18" and he's about 4ft tall.

    Is there any hope for me to obtain these goals this year? What would you suggest oh robotic gurus and geniuses?


    Sincerely,
    the Perigalacticon

  2. #2

    Re: Creeper needs attack mode

    You don't need SLAM, because you can already build a map ahead of time.

    You might want to use something like a couple of ultrasonic sensors to measure distances to edges, and perhaps a magnetometer / IMU to figure out orientation, which will let you triangulate against the known walls to know where you're at.

    Even simpler would be to have something like an IR beacon blinking at a known frequency (say, 100 Hz so it's not confused with 60 Hz) and detect it and its strength to have a "home bearing" and don't get too far from that.

    If you have a little more cash, you can look at something like the POSZYX boards/transmitters to get a real location.

  3. #3

    Re: Creeper needs attack mode

    At a minimum, I want Curt to wander around my flat concrete driveway at idle, and maybe out onto the sidewalk and back. This sounds to me like it needs SLAM.
    perigalacticon, as this is a temporary application I could see laying down masking tape over the path, then
    setup the Minecraft Creeper prop as a two wheel drive line follower(other two wheels as casters), I could
    see using different colored masking tape to trigger a Minecraft Creeper prop action.

    example: if tape color is blue and ultrasonic sensor is less then(some value) the
    Minecraft Creeper prop turns on red
    light and stops.
    Last edited by Tommy_T; 01-24-2021 at 08:17 AM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) PWM Operating Mode
    By German Shepherd in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 05-29-2019, 02:40 AM
  2. Question(s) Using AX-12A in zero torque mode.
    By ZanQdo in forum DYNAMIXEL & Robot Actuators
    Replies: 9
    Last Post: 06-20-2015, 04:23 AM
  3. xbee api mode help!!
    By nondescript in forum Software and Programming
    Replies: 0
    Last Post: 06-10-2013, 07:54 PM
  4. Question(s) Creeper 2 Software Update
    By WGhost9 in forum Software and Programming
    Replies: 5
    Last Post: 01-02-2010, 02:20 AM
  5. Interesting "Lethal Injection Attack Droid Prototype"
    By archcvd in forum Off Topic
    Replies: 4
    Last Post: 05-03-2008, 06:03 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •