Page 21 of 22 FirstFirst ... 11171819202122 LastLast
Results 201 to 210 of 218

Thread: More Mule then Rover?

  1. Re: More Mule then Rover?

    seeing where you go is important :-)
    jwatte, nothing gives that warm&fuzzy feeling like good visibility.

    While I couldn't use the ballscrews I have available for the lifting of the bucket(too slow, small pitch)
    they may work out best for the dumping(only 10" travel)

    looking for a 4 sec. dump time(2 sec. down, 2 sec. back up)
    Last edited by Tommy_T; 12-10-2018 at 08:20 AM.

  2. Re: More Mule then Rover?

    smooth!


  3. Re: More Mule then Rover?

    with all the effort & costs that went into making the lifting frame, I'm going
    to install a second prox switch on each end of travel, that shuts down drive
    and turns on the brake.

    or the sabertooth drive has a current limiting pot, while it can lift 500lb+
    there's no reason to for snow. maybe just adjusting to a point where it
    can't damage the frame would be best?

  4. #204

    Re: More Mule then Rover?

    That looks awesome!

    You probably should do both current limiting and safety limit switches.

  5. Re: More Mule then Rover?

    Not sure about the plan A for dumping.

    the gear motor I plan to use has a 180rpm output, and the sprocket on the buckets
    only turns 90deg. to make it at least reasonable if things go sideways, I got 9 teeth
    on the motor 45 teeth on the dump shaft, then 12 teeth on the dump shaft output to
    the buckets 36 teeth sprocket, which should give it a 8 to 1 gear reduction.

    Click image for larger version. 

Name:	IMG_5111.jpg 
Views:	20 
Size:	124.2 KB 
ID:	7416

    Click image for larger version. 

Name:	IMG_5112.jpg 
Views:	20 
Size:	106.1 KB 
ID:	7417

    Click image for larger version. 

Name:	IMG_5114.jpg 
Views:	24 
Size:	110.3 KB 
ID:	7418

  6. Re: More Mule then Rover?

    hope to test the dumping setup this week(waiting on motor with brake)

    Click image for larger version. 

Name:	IMG_5116.jpg 
Views:	19 
Size:	139.5 KB 
ID:	7419
    Click image for larger version. 

Name:	IMG_5117.jpg 
Views:	19 
Size:	145.6 KB 
ID:	7420
    Click image for larger version. 

Name:	IMG_5119.jpg 
Views:	22 
Size:	102.5 KB 
ID:	7421
    Click image for larger version. 

Name:	IMG_5121.jpg 
Views:	22 
Size:	87.8 KB 
ID:	7422
    Click image for larger version. 

Name:	IMG_5123.jpg 
Views:	25 
Size:	101.6 KB 
ID:	7423

  7. Re: More Mule then Rover?

    to set the height of the blade I had these welded on($25.00 sweet!)
    for small casters and a orange plow marker flag(should show up on camera).

    Click image for larger version. 

Name:	IMG_5125.jpg 
Views:	20 
Size:	167.8 KB 
ID:	7424

    I'm going to one more shaft, 12 teeth and 45 teeth get a slower
    speed on the dumping setup.
    5
    Last edited by Tommy_T; 4 Weeks Ago at 02:22 PM.

  8. Re: More Mule then Rover?

    I was able to test the dumping drive setup.
    the speed is manageable but, even with a 1" shaft because of
    the amount it's unsupported on each end it acts like a leaf spring(crap).

    Click image for larger version. 

Name:	spring.jpg 
Views:	18 
Size:	75.7 KB 
ID:	7425

  9. Re: More Mule then Rover?


  10. #210

    Re: More Mule then Rover?

    Looks quite robust! Now all you need is another foot of snow ;-)

Thread Information

Users Browsing this Thread

There are currently 4 users browsing this thread. (0 members and 4 guests)

Similar Threads

  1. Project Second Rover Build
    By Sundsted in forum Rovers
    Replies: 3
    Last Post: 07-17-2010, 04:04 PM
  2. First rover bot project!
    By Carlcox89 in forum Rovers
    Replies: 4
    Last Post: 07-01-2010, 06:55 PM
  3. Fit-Bot - a Fit-PC based rover
    By coppertubing in forum Robot Computers
    Replies: 9
    Last Post: 10-06-2009, 09:32 AM
  4. Xan's Rover with Arm
    By Xan in forum Rovers
    Replies: 14
    Last Post: 07-18-2009, 02:16 AM
  5. Discussion Rover Kits
    By LinuxGuy in forum Rovers
    Replies: 0
    Last Post: 04-02-2008, 05:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •