Page 25 of 29 FirstFirst ... 15212223242526272829 LastLast
Results 241 to 250 of 287

Thread: More Mule then Rover?

  1. #241

    Re: More Mule then Rover?

    With the bigger motor it's pointing up and is visible in the camera facing
    down on the bucket attachments.

    when I get back to Wisconsin Sunday I'll post video of it bouncing around

    this week I'm in San Francisco for work, if they got snow here they would be screwed
    with these steep angle streets.

  2. #242

    Re: More Mule then Rover?

    Click image for larger version. 

Name:	IMG_5364.jpg 
Views:	233 
Size:	113.0 KB 
ID:	7461

    the flexing of this aluminum bracket is due to
    the 6" distance between the mounting bolts and
    the chain sprocket.

    Click image for larger version. 

Name:	IMG_5363.jpg 
Views:	230 
Size:	110.9 KB 
ID:	7462

    it could be minimized with a gusset added.

    I'll test what would happen if a limit switch fails
    after I change it to steel.

  3. #243

    Re: More Mule then Rover?

    That sounds exciting!

    Curiousity killing cats:
    How is the "L" part attached? Welded?
    How thick is the plate that the bolts go through?

  4. #244

    Re: More Mule then Rover?

    jwatte, the current motor bracket is made from 2pc .5" x 2.5" 6061 aluminium plate.
    the plates are bolted together by (4) 1/4-20 SHCS (grade 8) .

  5. #245

    Re: More Mule then Rover?

    I'm also not happy with the bracket design when used with the bigger motors.

    these bigger motors have OEM mounting holes (6-M6 tapped holes), but I added
    (8) 10-32 tapped holes to be able used the current bracket design and current
    chain length.

    I have 6 of these motors sitting around, but only one that has a 10-32 bolt circle.

    if I have to swap motors it would be a pain.
    Last edited by Tommy_T; 03-04-2019 at 08:52 PM.

  6. #246

    Re: More Mule then Rover?

    I just looked up and noticed that it's march.
    time to turn attention to mowing, big build this season for dealing with grass.

    Lots of fun this winter! looking forwards to next winter.
    the bucket turned out to be a very useful attachment.

  7. #247

    Re: More Mule then Rover?

    the bucket also makes changing mower blades easier.

    Click image for larger version. 

Name:	IMG_5425.jpg 
Views:	203 
Size:	137.7 KB 
ID:	7468

    Click image for larger version. 

Name:	IMG_5427.jpg 
Views:	206 
Size:	109.8 KB 
ID:	7469

  8. #248

    Re: More Mule then Rover?

    It's a robot controlled lift! Stylish!

  9. #249

    Re: More Mule then Rover?

    I do get this is a deadhorse type topic, but.

    I got big plans for the mule this fall and winter.

    the picture in my head for this next build(all wheel drive) has changed from
    just last winter. I now see adding two smaller wheels in front of the current
    drive system.

    Click image for larger version. 

Name:	IMG_5841.jpg 
Views:	173 
Size:	123.9 KB 
ID:	7593

    the reason for the change is all about balance, the bucket attechment weights
    over 200lb empty, because of the other big change is I'm not adding batteries to offset
    the weight of the attechment, I'm adding a 6hp gas engine with electric start to run a
    100amp 24vdc alternator to charge the current batteries.
    Last edited by Tommy_T; 08-07-2019 at 09:57 PM.

  10. #250

    Re: More Mule then Rover?

    I was wondering how the linear guides wound hold up in the harsh wisconsin
    environment.

    image below is after one winter.

    Click image for larger version. 

Name:	IMG_5842.jpg 
Views:	196 
Size:	110.9 KB 
ID:	7594

Thread Information

Users Browsing this Thread

There are currently 7 users browsing this thread. (0 members and 7 guests)

Similar Threads

  1. Project Second Rover Build
    By Sundsted in forum Rovers
    Replies: 3
    Last Post: 07-17-2010, 04:04 PM
  2. First rover bot project!
    By Carlcox89 in forum Rovers
    Replies: 4
    Last Post: 07-01-2010, 06:55 PM
  3. Fit-Bot - a Fit-PC based rover
    By coppertubing in forum Robot Computers
    Replies: 9
    Last Post: 10-06-2009, 09:32 AM
  4. Xan's Rover with Arm
    By Xan in forum Rovers
    Replies: 14
    Last Post: 07-18-2009, 02:16 AM
  5. Discussion Rover Kits
    By LinuxGuy in forum Rovers
    Replies: 0
    Last Post: 04-02-2008, 05:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •