Page 16 of 24 FirstFirst ... 6121314151617181920 ... LastLast
Results 151 to 160 of 231

Thread: More Mule then Rover?

  1. #151

    Re: More Mule then Rover?

    yet the snow bucket is still not installed
    Well, who's fault is that?

    It seems I'm the reason for the slow down
    Oh, right then.

    What fun would it be without overthinking? :-)

    Else you would just weld a 3/8" steel plate on front at a diagonal, that would plow just fine as long as you keep up when it's coming down. No fun in that. (Other than saving the work of doing the plowing manually.)

  2. #152

    Re: More Mule then Rover?

    What fun would it be without overthinking? :-)
    jwatte, I'm still scratching my head about what type drive to use to lift the bucket.
    I have a ballscrew from a bridgeport mill, but with a pitch of .200" and a motor with 180rpm
    it would take some time to lift the bucket(@20sec. with 4 to 1 gearing of the gearbox).

    if I went to a chain drive, I could get it down to 5sec.

  3. #153

    Re: More Mule then Rover?

    Also, could you bolt lifting arms to the side, to give you a longer lever? Put the pivot point at the back of the bot, lift somewhere in the middle, and put the bucket in front, for additional speed gain (and, of course, torque loss, so that counteracts your 4:1 gearbox ...)
    Really, just add a harder/better/faster/stronger motor and call it good, I guess? :-D

    I think this is why professional gear uses hydraulics... Build high pressure in a storage tank, use it when needed to actuate with high forces quickly, as long as you're OK with some mush in the system and some lag in the control loop.

    Also, how far do you really need to lift the bucket? You don't really need to lift it much more than the regular ground clearance of the 'bot, right?

  4. #154

    Re: More Mule then Rover?

    how far do you really need to lift the bucket?
    jwatte, with the way the bucket was made I have to lift it 18" just to dump it.
    I'm thinking of lifting a total of 34".

    I think this is why professional gear uses hydraulics.
    jwatte, this is where the overthinking come in...
    hydraulics would be a easy to implement setup, I can get stuff at farm&fleet to do the job.
    but, I need to start playing at 5 am so I can still get some work done that day, and with 30
    neighbors that would be in range of the sounds the hydraulic pump, they may not let me play
    in their space at that time. (that would suck!)

    I have the same issue with electric winches.(too loud)
    Last edited by Tommy_T; 11-12-2018 at 07:42 AM.

  5. #155

    Re: More Mule then Rover?

    30 neighbors that would be in range of the sounds the hydraulic pump
    My neighbors don't worry about their lawn crews using weed trimmers at 6am, soo ....
    Buy a shotgun, ignore the neighbors? :-D

  6. #156

    Re: More Mule then Rover?

    for the first try, I'm going with a #50 chain for the bucket lift and bucket dump drives systems.
    Click image for larger version. 

Name:	IMG_5012.jpg 
Views:	20 
Size:	114.4 KB 
ID:	7341


    I'm going to have the frame welded together this week.

    baby steps.

  7. #157

    Re: More Mule then Rover?

    Ooh, those look like linear guides! That is, indeed, overkill ;-)

  8. #158

    Re: More Mule then Rover?

    Ooh, those look like linear guides! That is, indeed, overkill ;-)
    jwatte, have to agree with you on that one, but it should be a very quiet lift.

    the motors I planed to use for the lift&dump systems were motors I had
    used a few years ago for an electric bike project(very fun project).
    Click image for larger version. 

Name:	tt6.jpg 
Views:	19 
Size:	146.2 KB 
ID:	7342

    but, it seems I removed the electric brakes from them(crap!)
    and for the lift& dump systems brakes are needed.

    back to ebay.
    Last edited by Tommy_T; 11-19-2018 at 05:57 AM.

  9. #159

    Re: More Mule then Rover?

    when I started the mule project for convenience I had two battery groups,
    12vdc and 24vdc with two different charging systems.

    the 12vdc for PC , cameras and lighting, and 24vdc for the motor drives.

    this year all batteries are going to be in one group, 24vdc.

    (4) 12vdc 100ah batteries.

    Click image for larger version. 

Name:	12vdc.jpg 
Views:	22 
Size:	130.5 KB 
ID:	7343

    I'm also removing the PC(in the mule) and replacing with 2 Arduino Nano,
    and replacing the wifi control communications with an Xbee.


    while I should have some fixed 24vdc to 12vdc/5vdc regulators show up
    this week, I'm still installing a 24vdc to 110vac inverter in case I need to
    run an air compressor,110vac lighting or heater.
    Last edited by Tommy_T; 11-19-2018 at 08:01 AM.

  10. #160

    Re: More Mule then Rover?

    the only time I've had Arduino's lock up on me are when
    I have serial port conflicts, so even with using 2 Arduinos(one is for safety checks)
    I'm going to use I2c 16bit DAC(0-5vdc) for controlling all the drives, I2c 16bit ADC(0-5vdc)
    for feedback.

    Click image for larger version. 

Name:	muleboard1.jpg 
Views:	21 
Size:	113.1 KB 
ID:	7344
    Last edited by Tommy_T; 11-19-2018 at 01:13 PM.

Thread Information

Users Browsing this Thread

There are currently 3 users browsing this thread. (0 members and 3 guests)

Similar Threads

  1. Project Second Rover Build
    By Sundsted in forum Rovers
    Replies: 3
    Last Post: 07-17-2010, 04:04 PM
  2. First rover bot project!
    By Carlcox89 in forum Rovers
    Replies: 4
    Last Post: 07-01-2010, 06:55 PM
  3. Fit-Bot - a Fit-PC based rover
    By coppertubing in forum Robot Computers
    Replies: 9
    Last Post: 10-06-2009, 09:32 AM
  4. Xan's Rover with Arm
    By Xan in forum Rovers
    Replies: 14
    Last Post: 07-18-2009, 02:16 AM
  5. Discussion Rover Kits
    By LinuxGuy in forum Rovers
    Replies: 0
    Last Post: 04-02-2008, 05:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •