Page 17 of 21 FirstFirst ... 7131415161718192021 LastLast
Results 161 to 170 of 207

Thread: More Mule then Rover?

  1. #161

    Re: More Mule then Rover?

    Are those Teensy 2 boards on the sides? Or some Arduino Leonardo clones, perhaps?

  2. Re: More Mule then Rover?

    Are those Teensy 2 boards on the sides?
    jwatte, they are Arduino Nano V3.1 boards

    https://www.mouser.com/ProductDetail...XAYdh8vxKmOPAO
    Last edited by Tommy_T; 4 Weeks Ago at 02:30 PM.

  3. #163

    Re: More Mule then Rover?

    Ah, yes, and you even said so in your post!

  4. Re: More Mule then Rover?

    While waiting on parts for the bucket build I should think about
    rebuilding the current handheld mule remote controller.

    It's in a very sad shape.

    Click image for larger version. 

Name:	IMG_5023.jpg 
Views:	12 
Size:	127.5 KB 
ID:	7346

  5. Re: More Mule then Rover?

    lucky for me, I had someone else weld the frame for me.
    and it turned out very sweet!.
    (if I did it, even using cold rolled steel it would have been spaghetti.)

    Click image for larger version. 

Name:	frame1.jpg 
Views:	10 
Size:	130.8 KB 
ID:	7347

    plan A
    Click image for larger version. 

Name:	frame2.PNG 
Views:	11 
Size:	8.7 KB 
ID:	7348
    plan B

    Click image for larger version. 

Name:	frame3.PNG 
Views:	10 
Size:	9.2 KB 
ID:	7349
    Last edited by Tommy_T; 3 Weeks Ago at 05:42 PM.

  6. Re: More Mule then Rover?

    Baby steps.
    Click image for larger version. 

Name:	IMG_5028.jpg 
Views:	13 
Size:	103.6 KB 
ID:	7350

    Click image for larger version. 

Name:	IMG_5030.jpg 
Views:	11 
Size:	194.2 KB 
ID:	7351

    Click image for larger version. 

Name:	IMG_5032.jpg 
Views:	10 
Size:	91.5 KB 
ID:	7352

    Click image for larger version. 

Name:	IMG_5033.jpg 
Views:	8 
Size:	94.3 KB 
ID:	7353

  7. Re: More Mule then Rover?

    baby steps.

    Click image for larger version. 

Name:	IMG_5034.jpg 
Views:	11 
Size:	138.2 KB 
ID:	7354

    Click image for larger version. 

Name:	IMG_5036.jpg 
Views:	11 
Size:	120.2 KB 
ID:	7355

  8. #168

    Re: More Mule then Rover?

    Did you cut that circular pocket on a manual mill without a rotary table? Or are there stepper motors somwhere I'm not seeing them? :-D

  9. Re: More Mule then Rover?

    Did you cut that circular pocket on a manual mill without a rotary table?
    Jwatte, that's one of the things that makes the 1.5 hour drive(each way) to the office worth
    the drive, the Mill has a conversational control on it(very sweet!), a lathe, surface grinder,
    and Steel in the stock rack(life is good).

    the ability to mill bearing seats or turn snap ring grooves comes in very handy with this type project.
    Click image for larger version. 

Name:	IMG_4075.jpg 
Views:	9 
Size:	121.8 KB 
ID:	7358

    Click image for larger version. 

Name:	IMG_5031.jpg 
Views:	10 
Size:	113.6 KB 
ID:	7356

    Click image for larger version. 

Name:	IMG_4300.jpg 
Views:	11 
Size:	143.9 KB 
ID:	7357
    Last edited by Tommy_T; 3 Weeks Ago at 08:25 AM.

  10. Re: More Mule then Rover?

    I only have a single axis motor drive sitting around(sabertooth 50), and
    I can't see a need to lift and dumping at the same time. so I got
    a 80A DPDT 24vdc relay to switch between motors(lift/dump) using
    the single sabertooth motor Drive.

    to simplify the first setup, I'm going to have very basic controls for the lift/dump.

    (2) toggle switches
    (1) momentary push button

    one toggle switch for Up/Down for lift
    one toggle switch for Up/Dump for bucket
    the momentary switch is an enable button.

    I have (4) 5vdc NPN inductive prox switches for each end of travels.
    Last edited by Tommy_T; 3 Weeks Ago at 09:22 AM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Second Rover Build
    By Sundsted in forum Rovers
    Replies: 3
    Last Post: 07-17-2010, 04:04 PM
  2. First rover bot project!
    By Carlcox89 in forum Rovers
    Replies: 4
    Last Post: 07-01-2010, 06:55 PM
  3. Fit-Bot - a Fit-PC based rover
    By coppertubing in forum Robot Computers
    Replies: 9
    Last Post: 10-06-2009, 09:32 AM
  4. Xan's Rover with Arm
    By Xan in forum Rovers
    Replies: 14
    Last Post: 07-18-2009, 02:16 AM
  5. Discussion Rover Kits
    By LinuxGuy in forum Rovers
    Replies: 0
    Last Post: 04-02-2008, 05:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •