Page 20 of 24 FirstFirst ... 10161718192021222324 LastLast
Results 191 to 200 of 231

Thread: More Mule then Rover?

  1. #191

    Re: More Mule then Rover?

    these passed the 24 hour heat test.
    Click image for larger version. 

Name:	IMG_5053.jpg 
Views:	26 
Size:	126.6 KB 
ID:	7376

    they also have a 200A version with the same foot print.
    which I'll most likely use when both sabertooth 2x60's are in use.

    when I made the motor mount brackets, I made all four at same time.
    but, not sure if I'll get all four installed this season(I'm slow).
    Click image for larger version. 

Name:	110917 055.jpg 
Views:	25 
Size:	108.1 KB 
ID:	7377
    Last edited by Tommy_T; 11-29-2018 at 07:27 AM.

  2. #192

    Re: More Mule then Rover?

    baby steps
    Click image for larger version. 

Name:	IMG_5057.jpg 
Views:	28 
Size:	129.1 KB 
ID:	7380

    Click image for larger version. 

Name:	IMG_5061.jpg 
Views:	28 
Size:	120.2 KB 
ID:	7381

    Click image for larger version. 

Name:	c2.PNG 
Views:	22 
Size:	939.7 KB 
ID:	7402 Click image for larger version. 

Name:	c3.jpg 
Views:	22 
Size:	75.2 KB 
ID:	7403

    I'm going to test lifting the bucket while still just bolted together, before I take it back
    to the welder. the bucket with dump motor and brackets is only 160lb.
    Attached Thumbnails Attached Thumbnails Click image for larger version. 

Name:	c4.PNG 
Views:	18 
Size:	1.12 MB 
ID:	7404  
    Last edited by Tommy_T; 11-30-2018 at 06:57 AM.

  3. #193

    Re: More Mule then Rover?

    "only"

  4. #194

    Re: More Mule then Rover?

    "only"
    Lucky for me I ordered a manufactured steel bucket(80lb) from Home Depot, if I made it,
    chances are it would weigh 300lb.(like the lifting frame I'm working on)

    there is lots of aluminium in the stock rack at work, but it's for current jobs, there's lots
    of steel that is left over from past jobs that I can use for free(free is good, but very heavy)

    with the bucket lift installed on the mule I shouldn't have to add any sand bags for weight
    to get traction.

    Click image for larger version. 

Name:	IMG_5064.jpg 
Views:	29 
Size:	119.1 KB 
ID:	7405
    Last edited by Tommy_T; 11-30-2018 at 09:55 PM.

  5. #195

    Re: More Mule then Rover?

    Free material is best material!
    (Or, as I prefer to think of it: Made of pure scrapbinium!)

  6. #196

    Re: More Mule then Rover?

    I should have the bucket mounted to the lift soon

    Click image for larger version. 

Name:	IMG_5066.jpg 
Views:	21 
Size:	106.1 KB 
ID:	7406

    Click image for larger version. 

Name:	IMG_5069.jpg 
Views:	22 
Size:	112.3 KB 
ID:	7407

    Click image for larger version. 

Name:	IMG_5071.jpg 
Views:	23 
Size:	90.3 KB 
ID:	7408

    Click image for larger version. 

Name:	IMG_5073.jpg 
Views:	24 
Size:	113.8 KB 
ID:	7409

  7. #197

    Re: More Mule then Rover?

    plan A is to use one 1000W motor for lifting and one for dumping.

    plan B is to use two 1000W motors for lifting and one for dumping.

    Click image for larger version. 

Name:	IMG_5084.jpg 
Views:	26 
Size:	116.8 KB 
ID:	7410

    Click image for larger version. 

Name:	IMG_5090.jpg 
Views:	25 
Size:	139.1 KB 
ID:	7411

    Click image for larger version. 

Name:	IMG_5092.jpg 
Views:	28 
Size:	129.0 KB 
ID:	7412

    Click image for larger version. 

Name:	IMG_5093.jpg 
Views:	174 
Size:	122.4 KB 
ID:	7413
    Last edited by Tommy_T; 12-02-2018 at 09:03 PM.

  8. #198

    Re: More Mule then Rover?

    the lift works as envisioned, 5 sec. for full lift height, tested lifting 290lb, it lifted
    it with no measurable slow down.(Sweet!) the braking system worked perfect also.

    everything very smooth, and very quiet.

    now for the dumping system.
    Last edited by Tommy_T; 12-03-2018 at 04:16 PM.

  9. #199

    Re: More Mule then Rover?

    baby steps.

    got the prox switches for the lift installed.

    Click image for larger version. 

Name:	IMG_5095.jpg 
Views:	24 
Size:	97.9 KB 
ID:	7415

    also moved the bucket out 2" to give me room to mount the dump
    motor under the bucket support arm(so it doesn't block camera view) .

  10. #200

    Re: More Mule then Rover?

    seeing where you go is important :-)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Second Rover Build
    By Sundsted in forum Rovers
    Replies: 3
    Last Post: 07-17-2010, 04:04 PM
  2. First rover bot project!
    By Carlcox89 in forum Rovers
    Replies: 4
    Last Post: 07-01-2010, 06:55 PM
  3. Fit-Bot - a Fit-PC based rover
    By coppertubing in forum Robot Computers
    Replies: 9
    Last Post: 10-06-2009, 09:32 AM
  4. Xan's Rover with Arm
    By Xan in forum Rovers
    Replies: 14
    Last Post: 07-18-2009, 02:16 AM
  5. Discussion Rover Kits
    By LinuxGuy in forum Rovers
    Replies: 0
    Last Post: 04-02-2008, 05:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •