Page 2 of 2 FirstFirst 12
Results 11 to 20 of 20

Thread: my own spin on the Phantom X

  1. Re: my own spin on the Phantom X

    Quote Originally Posted by lnxfergy View Post
    No. You're not going to run OpenCV on the ArbotiX -- or anything but an Intel based PC. What you can do is run OpenCV on a laptop/PC and then use the ArbotiX to interface the laptop/PC to your servos and other hardware. This is exactly what that demo of the PhantomX is doing -- except with roborealm on the PC rather than OpenCV. You would communicate with the ArbotiX over a serial port connection from your PC-side program (hence Adrenalynn's comment that dotNet can open serial port).

    -Fergs
    that's exactly what I told the Arduino people! well thanks for the useful information, so far you guys have helped a ton and I can't wait to get started on my project

  2. Re: my own spin on the Phantom X

    I have one more question about the Arbotix boards that I can't find an answer for: can I use Arduino libraries and or source code on an Arbotix? if so what change(s) need to be made for it to work?

  3. #13
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    135

    Re: my own spin on the Phantom X

    Quote Originally Posted by ahack3r View Post
    I have one more question about the Arbotix boards that I can't find an answer for: can I use Arduino libraries and or source code on an Arbotix? if so what change(s) need to be made for it to work?
    Depends on the library -- if it uses only the basic arduino interfaces (digitalWrite, digitalRead, etc) it should run fine. If it makes reference to registers -- it probably will require updates to work on the different AVR that the ArbotiX uses.

    -Fergs

  4. Re: my own spin on the Phantom X

    Quote Originally Posted by lnxfergy View Post
    Depends on the library -- if it uses only the basic arduino interfaces (digitalWrite, digitalRead, etc) it should run fine. If it makes reference to registers -- it probably will require updates to work on the different AVR that the ArbotiX uses.

    -Fergs
    and where would I obtain these specific updates?

  5. #15
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    149

    Re: my own spin on the Phantom X

    Quote Originally Posted by ahack3r View Post
    and where would I obtain these specific updates?
    Here's looking at you kid.

  6. #16
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    135

    Re: my own spin on the Phantom X

    Quote Originally Posted by ahack3r View Post
    and where would I obtain these specific updates?
    The core libraries (serial, twi, spi, etc) have been updated already -- they come with the ArbotiX downloads. Additionally, we publish the RoboController libraries for controlling specific hardware on the MINI and ArbotiX. Beyond that, if you want to use a custom third-party library, you'll need to look into the code to see if it needs changes, and then apply them yourself.

    -Fergs

  7. Re: my own spin on the Phantom X

    Quote Originally Posted by lnxfergy View Post
    The core libraries (serial, twi, spi, etc) have been updated already -- they come with the ArbotiX downloads. Additionally, we publish the RoboController libraries for controlling specific hardware on the MINI and ArbotiX. Beyond that, if you want to use a custom third-party library, you'll need to look into the code to see if it needs changes, and then apply them yourself.

    -Fergs
    awesome! thanks for the information, it will help tremendously.

  8. Re: my own spin on the Phantom X

    sorry to resurrect a dead thread

    I have two more questions:


    1. when will the Visual C# .NET Sample Application & Source and Roborealm Colored Object Tracking Demo be posted? I would really like to have this documentation before purchasing.
    2. what webcams are compatible with the Arbotix and ROS? I will be using the OpenCV library.
    3. I will be using Ubuntu 10.10, what changes do I need to make?



    thanks!
    Last edited by ahack3r; 11-07-2010 at 03:59 PM.

  9. #19
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    135

    Re: my own spin on the Phantom X

    Quote Originally Posted by ahack3r View Post
    when will the Visual C# .NET Sample Application & Source and Roborealm Colored Object Tracking Demo be posted? I would really like to have this documentation before purchasing.
    I can't answer this one as I'm not the developer -- but you might shoot an email to Alex at Trossen Robotics to find out.

    what webcams are compatible with the Arbotix and ROS? I will be using the OpenCV library.
    The ArbotiX knows nothing about webcams, that's all handled up on a PC. Therefore, you're looking at what is supported by ROS or OpenCV. Any webcam that has decent V4L support should work under Linux.

    I will be using Ubuntu 10.10, what changes do I need to make?
    Well, neither roborealm nor the C# code are going to work.... As for ROS, I'm not sure the status of the binaries for installation under 10.10 -- last I knew, they weren't complete for cturtle.

    -Fergs

  10. Re: my own spin on the Phantom X

    Quote Originally Posted by lnxfergy View Post
    I can't answer this one as I'm not the developer -- but you might shoot an email to Alex at Trossen Robotics to find out.



    The ArbotiX knows nothing about webcams, that's all handled up on a PC. Therefore, you're looking at what is supported by ROS or OpenCV. Any webcam that has decent V4L support should work under Linux.



    Well, neither roborealm nor the C# code are going to work.... As for ROS, I'm not sure the status of the binaries for installation under 10.10 -- last I knew, they weren't complete for cturtle.

    -Fergs
    well...thanks for the webcam info I'm glad I haven't formatted my win7 partition yet!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Lottery Wheel
    By POTMO in forum Robotics General Discussion
    Replies: 5
    Last Post: 04-14-2009, 11:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •