I have one more question about the Arbotix boards that I can't find an answer for: can I use Arduino libraries and or source code on an Arbotix? if so what change(s) need to be made for it to work?
The core libraries (serial, twi, spi, etc) have been updated already -- they come with the ArbotiX downloads. Additionally, we publish the RoboController libraries for controlling specific hardware on the MINI and ArbotiX. Beyond that, if you want to use a custom third-party library, you'll need to look into the code to see if it needs changes, and then apply them yourself.
-Fergs
my blog: http://www.ShowUsYourSensors.com
sorry to resurrect a dead thread
I have two more questions:
- when will the Visual C# .NET Sample Application & Source and Roborealm Colored Object Tracking Demo be posted? I would really like to have this documentation before purchasing.
- what webcams are compatible with the Arbotix and ROS? I will be using the OpenCV library.
- I will be using Ubuntu 10.10, what changes do I need to make?
thanks!
Last edited by ahack3r; 11-07-2010 at 03:59 PM.
I can't answer this one as I'm not the developer -- but you might shoot an email to Alex at Trossen Robotics to find out.
The ArbotiX knows nothing about webcams, that's all handled up on a PC. Therefore, you're looking at what is supported by ROS or OpenCV. Any webcam that has decent V4L support should work under Linux.what webcams are compatible with the Arbotix and ROS? I will be using the OpenCV library.
Well, neither roborealm nor the C# code are going to work.... As for ROS, I'm not sure the status of the binaries for installation under 10.10 -- last I knew, they weren't complete for cturtle.I will be using Ubuntu 10.10, what changes do I need to make?
-Fergs
my blog: http://www.ShowUsYourSensors.com
There are currently 1 users browsing this thread. (0 members and 1 guests)
Bookmarks