Results 1 to 4 of 4

Thread: C# code for moving servos!

  1. C# code for moving servos!

    I found this link:
    http://forums.trossenrobotics.com/showthread.php?t=1668


    well, i went there to get the code and the code link doesn't work anymore. But here is my story. I have a project that requires me to have 4 servos. i am wanting 2 of them to be controlled by a toggle switch, which i'm doing in vb, that will move the servo to one position and hold with one button pressed and then when the other it moves back to the opposite side and turns off. the other 2 are just a button that when pressed will move the servo to one position for a couple of seconds and move back. I have not coded in c before, or really any programming language that involves pc applications, and i am now on a very tight time constraint. I only have a month to build my project and get the motors implemented. is there anyone that can help me out? it would be greatly appreciated.

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    176

    Re: C# code for moving servos!

    What servo controller are you using? That's the important question - followed by what servos...
    I Void Warranties´┐Ż

  3. Re: C# code for moving servos!

    I am using the pololu micro maestro servo controller, with regular RC servo motors. i have a test program that sets up connection to the controller, so all i need to do is add the c code to their pre-existing c code to run the commands. and it is programmed in c# btw

  4. Re: C# code for moving servos!

    I really just need a quick function/variables that do the action, and then i can change the function name and the variables to fit each button.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Discussion Parallel Leg Mechanism Design
    By DresnerRobotics in forum Humanoids, Walkers & Crawlers
    Replies: 87
    Last Post: 06-24-2012, 10:13 AM
  2. C# code for controlling servo with keyboard
    By bluegear in forum Software and Programming
    Replies: 15
    Last Post: 09-10-2010, 05:25 PM
  3. Bioloid Premium Kit with embedded C
    By Buell24 in forum Humanoids, Walkers & Crawlers
    Replies: 13
    Last Post: 06-02-2010, 12:50 PM
  4. C# Bioloid Motion Sequence Program
    By DresnerRobotics in forum Mech Warfare
    Replies: 4
    Last Post: 11-25-2009, 04:55 AM
  5. Easy Programing of servos and play back
    By hotrodled in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 01-30-2008, 03:18 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •