Page 2 of 2 FirstFirst 12
Results 11 to 13 of 13

Thread: Recommendations for high capacity Lithium ion battery packs?

  1. #11
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    141

    Re: Recommendations for high capacity Lithium ion battery packs?

    I guess I should clarify that Ive only dealt with two cheap brands previous to my thunderpower switch, but I've never been happier with the switch. I also like the option of using the milspec line, which is insanely light/compact. Definitely can't compare genetics there, but they're spendy.

    I'm all for disagreement Billy! At least you cite your sources.

  2. #12
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    49

    Re: Recommendations for high capacity Lithium ion battery packs?

    Thanks for the suggestions. Safety *is* one of my top priorities since every time I recharge my current lipos I wonder if this is the time I burn the house down...The LiFePO were new to me and it sounds like they are much safer than lipos. Also, in terms of capacity, I am looking for something at least 10000mAh in a single battery so I can run the robot for several hours on a charge and I only have to charge one battery, use one DC-DC converter, etc. Seems that Hobby City tops out at around 4500mA per battery. The ThunderPower site lists lipos up to 8000 mA but not LiFePO as far as I can see.

    --patrick
    The Pi Robot Project
    http://www.pirobot.org

  3. #13
    Join Date
    Aug 2008
    Location
    Iowa City, IA
    Posts
    390
    Rep Power
    46

    Re: Recommendations for high capacity Lithium ion battery packs?

    Well if weight is not a super concern, then A123 packs it is! With a Dewalt pack and two more cells you could make a 3S4P pack that is 9.9V nominal and 10400mAh for 840g in cells.

    btw. You can parallel charge your lipo packs.
    http://www.rcgroups.com/forums/showthread.php?t=932319

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) exceeded DPDT Switch's rating = very hot battery
    By kfrench in forum Power
    Replies: 16
    Last Post: 12-14-2009, 07:40 PM
  2. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 06:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •