Results 1 to 6 of 6

Thread: ArbotiX baud rate(s)?

  1. #1
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    54

    ArbotiX baud rate(s)?

    Hey Fergs,

    Am I correct in assuming that the ArbotiX connects only at 38400 baud? I just discovered that the Serializer (version 2.0) connects at every baud rate *but* 38400! I was planning on using a three node XBEE setup with the PC node beaming to both boards. But I'm guessing I have to run everything at the same baud rate which now does not seem possible...

    --patrick
    The Pi Robot Project
    http://www.pirobot.org

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    132

    Re: ArbotiX baud rate(s)?

    You can change to a different baud rate -- you just have to change the firmware (right in setup() change 38400 to something else in the line serial.begin(38400)).

    The reason we chose 38400 is because that is the speed that the bootloader runs at -- and so if you want to do wireless upload of code, 38400 is the baud needed. Other tools, such as PyPose will also need mods to run at something other than 38400 (has to currently be done in the code), however it's very easy to change to a different baud rate under the ROS package (can be set through the parameter server as /arbotix/baud)

    -Fergs

  3. #3
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    54

    Re: ArbotiX baud rate(s)?

    Fantastic!

    --p
    The Pi Robot Project
    http://www.pirobot.org

  4. #4
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    54

    Re: ArbotiX baud rate(s)?

    Just wanted to share a picture of Pi Robot with his new ArbotiX jet pack on.

    The Pi Robot Project
    http://www.pirobot.org

  5. #5
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    132

    Re: ArbotiX baud rate(s)?

    Ok, I realize this is a bit of thread hijacking -- but I think we've solved the original issue so it's OK. Do you have any more photos of the construction of the omnidirectional camera? I've got a pile of christmas ornaments here that are begging to get put to use (the first construction, with coathangers and cardboard wasn't too robust).

    I know you're using clear plastic tube, but how do you attach at the top and bottom to make it rigid?

    -Fergs

  6. #6
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    54

    Re: ArbotiX baud rate(s)?

    Here are a few more pics. Note that the mirror is no longer a Christmas ornament but a hyperbolic mirror I had custom made so I could more easily mount it this way. However, the image quality is not much better than a good ornament and if you could saw the ornament in half, it should work just as well.

    I got the tubing online from McMaster:

    http://www.mcmaster.com/#8486k457/=8tjlpl

    (The tubing from Tap Plastics does not have sufficient optical clarity for this application--in fact it has very visible vertical streaks that severely distort the image.)

    The camera is a USB Philips SPC1300NC stuck to a plastic plate from Tap Plastics using carpet tape. It has a manual focus ring which helped when putting the mirror that close to the lens. The bottom plate and top disc (on top of the tube) are also from TP. The mirror is bolted to the top plate while the plate itself is glued to the tube.

    --patrick
    The Pi Robot Project
    http://www.pirobot.org

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. The Ultimate Arbotix Thread
    By sthmck in forum Arbotix, Microcontrollers, Arduino
    Replies: 53
    Last Post: 08-29-2011, 08:41 AM
  2. Question(s) Newby Arbotix hassles
    By Slugman in forum Robot Computers
    Replies: 29
    Last Post: 11-15-2010, 08:52 AM
  3. Question(s) Arbotix problems with pose servo position
    By muc in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 02-21-2010, 06:11 PM
  4. XBee Baud rates.
    By KurtEck in forum Arbotix, Microcontrollers, Arduino
    Replies: 6
    Last Post: 10-27-2009, 07:55 PM
  5. "ALMower" [was: Robotic Lawn Mower]
    By revoltage in forum Robotics General Discussion
    Replies: 363
    Last Post: 07-19-2009, 08:06 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •