Results 1 to 6 of 6

Thread: quadrocopter w/ROS Arbotix

  1. quadrocopter w/ROS Arbotix

    what are your thoughts on using ROS arbotix on a quadrocopter/UAV like robot? I love the PIXHawk here http://www.ros.org/news/2010/09/robo...licopters.html but instead of using their board, I would use the Arbotix...is this possible?

  2. #2
    Join Date
    Nov 2007
    Posts
    397
    Images
    71
    Rep Power
    59

    Re: quadrocopter w/ROS Arbotix

    from a purely electronics stand point it would be. You would have to use ESC to control the motors and you would have to find an IMU that you could get working with the arbotix. As far as what you would be doing with ROS I have no idea how that would work. If you check out diydrones.com you should be able to find some info on arduino controlled quad copters which is essentially what you want to do here.

  3. #3
    Join Date
    Feb 2010
    Location
    Silicon Valley, CA
    Posts
    321
    Images
    1
    Rep Power
    48

    Re: quadrocopter w/ROS Arbotix

    ahack3r, we love ArbotiX here, but what's the reason for you not wanting to use their board?

  4. Re: quadrocopter w/ROS Arbotix

    Quote Originally Posted by sthmck View Post
    from a purely electronics stand point it would be. You would have to use ESC to control the motors and you would have to find an IMU that you could get working with the arbotix. As far as what you would be doing with ROS I have no idea how that would work. If you check out diydrones.com you should be able to find some info on arduino controlled quad copters which is essentially what you want to do here.
    yes, I'm looking into the Arducopter, thanks!

    Quote Originally Posted by RobotNV View Post
    ahack3r, we love ArbotiX here, but what's the reason for you not wanting to use their board?
    for two reasons:
    1. their site isn't responding.
    2. I want the functionality of the Arbotix for later projects.

  5. #5
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    134

    Re: quadrocopter w/ROS Arbotix

    Quote Originally Posted by ahack3r View Post
    what are your thoughts on using ROS arbotix on a quadrocopter/UAV like robot? I love the PIXHawk here http://www.ros.org/news/2010/09/robo...licopters.html but instead of using their board, I would use the Arbotix...is this possible?
    Possible? Yes.
    Easy? No.

    You'd have to develop your own firmware -- these quadrotors don't have enough payload to carry a PC, and over-the-air isn't going to be fast nor deterministic enough to do control of a quadrotor. While I'd love to see an ArbotiX-based quadrotor -- I have to admit it is probably the wrong tool for the job. Lots of other boards have been developed specifically for doing quadrotors/uavs, and it would be a much simpler job to add an ROS interface to one of these than.

    -Fergs

  6. Re: quadrocopter w/ROS Arbotix

    Quote Originally Posted by lnxfergy View Post
    Possible? Yes.
    Easy? No.

    You'd have to develop your own firmware -- these quadrotors don't have enough payload to carry a PC, and over-the-air isn't going to be fast nor deterministic enough to do control of a quadrotor. While I'd love to see an ArbotiX-based quadrotor -- I have to admit it is probably the wrong tool for the job. Lots of other boards have been developed specifically for doing quadrotors/uavs, and it would be a much simpler job to add an ROS interface to one of these than.

    -Fergs
    I have to agree, I've been doing even more research and came to the same conclusion...I guess I will have to keep my Turret and uav projects separate, for now

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Arbotix & PyPose
    By Suicidal.Banana in forum Software and Programming
    Replies: 90
    Last Post: 12-21-2017, 04:12 PM
  2. The Ultimate Arbotix Thread
    By sthmck in forum Arbotix, Microcontrollers, Arduino
    Replies: 53
    Last Post: 08-29-2011, 08:41 AM
  3. ArbotiX ROS Package 0.3.0
    By lnxfergy in forum ROS - Robot Operating System
    Replies: 233
    Last Post: 02-06-2011, 11:36 AM
  4. Question(s) Newby Arbotix hassles
    By Slugman in forum Robot Computers
    Replies: 29
    Last Post: 11-15-2010, 08:52 AM
  5. Question(s) Arbotix problems with pose servo position
    By muc in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 02-21-2010, 06:11 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •